Part Number: TPS735 Tool/software: Hi team,
Could you please let me know below devices are monolithic or not?
TPS386000RGPR
REF35330QDBVR
TPS3711DDCR
TPS3702CX33DDCR
TPS51206DSQR
TPS3702CX12DDCR
TPS73533DRVR…
Part Number: TPS735-Q1 Other Parts Discussed in Thread: TPS735 Hi team,
The package of TPA735 and TPS735-Q1 are a little difference.
The customer want to use TPS735 replace TPS735-Q1 without changing PCB. Is that ok?
thanks. : )
regards,
Ca…
Part Number: TPS735 Hi,
I have a customer using TPS73501DRB, and he wants to know whether the soft start time of this chip is adjustable, if so, how much capacitance is needed to adjust to at least 100us, is there a reference formula?
Many thanks…
Part Number: TPS735-Q1 I am conducting the FMEDA for an ECU that uses TPS73515QDRBRQ1. Please may I have the component fit rate as per SN 29500 and the FMD aswell.
Thank you,
Bushra
Part Number: TPS735 Hi,
Due to the customer's circuit design, the input voltage becomes 0 V⇔ about 1.5 V before the TPS735 starts.
At this time, is the voltage output from the OUT pin (1 pin)?
When I look at the internal circuit, EN(5 pin) and UVLO…
Part Number: TPS735-Q1 Hi team,
My customer is carrying out FMEDA activity on one project and the manufacture number is TPS73512QDRBRQ1.
But I couldn ’ t find any functional safety information( failure rate, failure mode, failure distribution and…
Part Number: TPS735 Hi
I have a question about TPS73501DRVR EN turn on VS VOUT and EN turn off VS VOUT, from figure 18 shown in datasheet, the turn on time is about 50us, but there is no figure about turn off time, in my circuit the COUT=22uF, can you…
Part Number: TPS735-Q1 Other Parts Discussed in Thread: USB2ANY , LMK3H0102 Tool/software: Here is my circuit which powers my clock generator LMK3H0102 which draws ~65 mA. I have a software based VOUT control by using a MOSFET driven by USB2ANY GPIOs…
Part Number: TPS735 The Vin and EN are connected together, the power on sequence is as follows.
the yellow waveform is Vout, blue waveform is Vin, why does Vout follow Vin when the EN pin is less than the threshold voltage? I think that Vout should…