Part Number: TPS736 Other Parts Discussed in Thread: TPS731 Hello guys,
One of my customers was going to use TPS73115 for their new product mass-productions.
But they knew it was difficult to prepare the device by their due date because TPS73115 lead time…
Hi Alon,
Stephen is OoO this week, but I have re-answered your question on the original thread for completeness.
In short there is no concern for TPS736 if Vin<Ven<=5.5V.
Part Number: TPS736 Could you offer the thermal derating information @Vout=3.3V? The curve diagram is Ambient temp versus Output Current.
application: Encoder for Motor drive
Working Ambient Temp: 105degree
Regards
Brian W
Hi Jamel,
1) The 5V is for a sensor. But this sensor also need 6V voltage for programming. This voltage is brought externally by the programming probe, but it means it will backpower the TPS73601 output. Is there a risk of damaging LDO with that ? If…
Part Number: TPS736-Q1 Other Parts Discussed in Thread: TPS736 Hi,
TPS736-Q1 use adjustable Output, TPS73601QDBVRQ1 ,it -supply the COMS SENSOR , Input 3.3V,output 1.8V& 2.8V , Applications is ADAS camera .
now,output 2.8V cannot be started,when COMS SENSOR…
Part Number: TPS736 Hi
I was looking at the datasheet of the TPS736 and specially the typical application section it says that there is a minimum of output current (20 mA for the fixed voltage version, 10 mA for the adjustable). I read about it but I…
Part Number: TPS736 Other Parts Discussed in Thread: TPS763 Hi,
Thanks for the previous explanation. I was wondering if the equivalent resistance network would be similar for a TPS736 device? Again, this is for the calculation of the DC output impedance…
Part Number: TPS736 Other Parts Discussed in Thread: TPS746 , TPS745 , TLV757P , TLV755P Hello team,
my customer has been using the TPS73601DRBT for a long time in order to power a Vcore physical Ethernet. Now they are redesigning the same family of product…