Part Number: TPS736 Hi team,
I have some question of TPS73601 as below. Especially, load regulation.
1. VFB is 1.198 to 1.21V at Tj = 25 deg. How much the VFB during Tj = -40 to 125 deg? I think 1%.
2. Unit of Load regulation mentioned %/mA. How to define…
Part Number: TPS736-Q1
Hi team,
This is Jessica, glad to work with you.
Could you please kindly help to recommend a LDO. The detail requirements is 3.3V output voltage, 300mA output current, and the package is SOT-895 for Automotive. Since i can't found…
Part Number: TPS736 Other Parts Discussed in Thread: TPS730 Hi,
1. The TPS736 datasheet have the separate specification for current Limit and short circuit current. But in many other datasheet have only current limit. I feel in TPS736, short circuit…
Part Number: TPS736 Hi,
Can you share the test procedure/testsetup for validating the Reverse leakage current, internal reference and output noise voltage of an LDO in bench testing.
Regards
Anuraj NK
Hello Terry,
TLV702-Q1 has a 2% DC output accuracy across temperature and a 0.5% at Tj = 25C. An alternative based on requirements is TPS736-Q1, it does not have output active discharge and the accuracy is 1% accuracy over line, load and temperature.…
Part Number: TPS736 I encounter problem when I use the TI download footprint for P/N "TPS73733DCQR", Allegro Netrev error as follow:
"ERROR(SPMHNI-195) Symbol 'DCQ6' for device 'TPS73733DCQR_DCQ6_TPS73733DCQR' is missing pin '6". Any quick solution…
Part Number: TPS736 Other Parts Discussed in Thread: TPS735 Hello,
We have a customer looking for the 1.2V Fixed Voltage option for the TPS736.
There is a reference to a 1.25V Fixed Output in the datasheet, however, in the product folder on ti.com, it…
Part Number: TPS736-Q1 Hi, Linear team
Do you have protection function about short to GND and short to battery on the TPS736-Q1?
Thanks
Best Regards
Gerald
Hi Kyle,
Could we know the difference between TPS736 and TPS730 family about the chip design for this issue?
Because we change the design to TPS730 family, we need to guarantee the part can work normally for our product.
Thank you!