Part Number: TPS73601-EP Hello,
We are considering replacing TPS73601DCQR with TPS73601DCQG4 due to part shortage. Are the parts able to be drop-in replicable, or are there any differences between the two materials?
If so, what are the differences?
Thank…
Part Number: TPS73601-EP Other Parts Discussed in Thread: TPS73801-SEP Hallo,
Is there radiation related (TID or SEE) test reports available for TPS73601MDCQREP. I could find a SEE report for TPS73601MDBVREP. Both are different packages. Along with this…
Hey Shengchang,
Given the device does not have an active pull down, adding a small amount of load to the output will help with the output voltage overshoots.
This is because the TPS73601-EP does not have an active pull down when the device goes too high…
Part Number: TPS73601-EP Other Parts Discussed in Thread: TPS736 Hi,
Can anyone specify the selected capacitance range of the optional output capacitor? What might be the maximum tolerable value as we found it affected the power-up of the microcontroller…
Part Number: TPS73601-EP Hi,
For the device TPS73601MDCQREP, the load transient response is mentioned in figure 30 for the out put voltage of 2.5V.
In the application I am using the ADJ LDO for the outputs 3.3V and 1.8V.
I would like to know the load transient…
Part Number: TPS73601-EP Hello teams,
I would like to know the quiescent current of TPS73601 when EN is high, and Vin from 1.7V to 5.5V, with certain output current. Is it so called "GND pin current", I am not shure because the value is hundreds uA..…
Part Number: TPS73601-EP Hi,
i have used TPS73601 DCQ package in my project. i amnot able to find the layout recommendations for this package in the datasheet.
Please provide these details.
Thank you
Ishank varshney
Part Number: TPS73601-EP Dear Sir or Madam
The TPS73601MDCQREP at our board is always outputting about 4V, when I measure the pin4(FB), it's about 1.6V .
here is my schematic, Are there anything wrong in my schematic ?I've also tried to changed to…
Part Number: TPS73601-EP Can I connect an external power supply of 1.2V to FB pin of the adjustable LDO (TPS73601DCQR) instead of programming the VFB using resistors, So that I can vary the output voltage as per the input.
Hi,
My customer is using TPS5430MDDAREP, TPS73133MDBVREP and TPS73601MDCQREP. He wants to know thermal resistance of these device. This thermal resistance is below. 1. Junction-to-case (top) thermal resistance 2. Junction-to-case (bottom) thermal resistance…