Part Number: TPS737 Hi team,
Regarding possible errors in the TPS737 datasheet, I would like to confirm the following two points:
In Figure 5-10, it is labeled as "Legacy silicon." Should this actually be "New silicon"?
In Figure 5-18, the unit…
Part Number: TPS737 Hello team,
My customer is consididering to apply DRB package for 5V->3.3V 550mA.
Do we have a guideline How copper area for thermal dissipation decide? I found the below note but if you have another idea, please let me know. …
Part Number: TPS737 Other Parts Discussed in Thread: TPS7E67-Q1 , Hello team,
Is the board design for Figure7-9 corresponding to 7.5.2 Layout Examples in the datasheet?
We want to see the case of DDA package (8pin) for comparison with TPS7E67-Q1…
Part Number: TPS737 While testing the IC TPS73701DRVR at 48 C for 18 days We observed that the output voltage of the REG is dropped from 2.9 to 1.8V on the 18th day. We tried changing the feedback parts but the issue remains. The problem solved when we…
Part Number: TPS737-Q1
Tool/software:
Hi, TI expert
I am trying to do a board layout using TPS73733QDRBRQ1.
However, when I checked the datasheet, there are two types of outline information: DRB0008A and DRB0008B.
When comparing DRB0008A and…
Part Number: TPS737 Tool/software: Hi team,
In PSpice simulation, my customer is seeing oscillation when inserting a 2.2uH ferrite bead at the input of TPS73701. When the bead parameter is changed to 0Ohm, the oscillation is disappeared. Please find…
Part Number: TPS737 Hi TI experts,
The design of TPS73701DRVR is shown below.
When TPS73701DRVR is powered off, the slow discharge of the Vout resulting a issue that the Vout is higher than the Vin.
Will this issue affect the chip, such as potentially…