Part Number: TPS73801-SEP Hello,
We order TPS73801-SEP and TPS7H4010MRNPTSEP parts.
We would like to have the TID results associated to the lots provided.
Is it possible to get it ?
Regards,
Guilhem
Part Number: TPS73801-SEP
Tool/software:
Hi,
is it feasible (if yes how) to use the TPS73801-SEP to generate an output voltage of 1V (i.e. less than 1.21V) ? If it's not feasible : what would be an alternative space enhanced (rad tolerant + plastic…
Part Number: TPS73801-SEP Hello, Looking at the minimum Vin spec, it is 2.2V, more than 1.9V(typ). It looks typo.
Actually, how much is the correct minimum Vin spec? Best regards, K.Hirano
Part Number: TPS73801-SEP Hello, My customer would like to have Transient Thermal Impedance plot data for TPS73801-SEP as follows.
Best regards, K.Hirano
Part Number: TPS73801-SEP Tool/software:
The AC model of the TPS73801-SEP shows peaking in the output impedance when a modulated load current is applied. Does the part actually behave like this?
Part Number: TPS73801-SEP Tool/software: Do we have data to help determine a worst-case drift over temperature for fixed loads and input voltages (such as a table?)
Thanks
Steve
Part Number: TPS73801-SEP Tool/software: Hello,
i have a question, why the SEP series has been assured as SEL 43MeV?
I want to know the reason of the standard(43 MeV).
Is it becasue of the orbit(LEO) analysis? or anything else?
Part Number: TPS73801-SEP Can we use the TPS73801-SEP when the input voltage is 5.45V?
Should we consider the derating rule based on the ECSS standards?
- Linear voltage regulator = Vin * 90%
ECSS-Q-ST-30-11C Rev.2: Derating – EEE components …
Part Number: TPS73801-SEP Tool/software: The SEE test report for the TPS73801-SEP shows that it was tested up to 43MeV-cm2 /mg.
Was this part tested up to 75MeV-cm2 /mg? And do you expect it to fail at that level?
Thank you.