Part Number: TPS73801-SEP Hi Team,
Hope you are well!
I have question regarding the TPS73801-SEP. The feedback reference voltage appears to have a maximum line regulation of 5 mV, and a maximum load regulation of 18 mV over the full range of temperatures…
Part Number: TPS73801-SEP Other Parts Discussed in Thread: TPS73801 ,
Hello,
I am working with TPS73801 in my design but I haven't found simulation model in TI site. I would know if someone could help me to simulate device behavior to get stability analysis…
Part Number: TPS73801-SEP
I've been looking at SLAK024 (TPS73801-SEP Single-Event Effects (SEE) Test Report) and the document appears incomplete - it references plots of the SETs observed but doesn't actually include them in the document.
I'm…
Part Number: TPS73801-SEP I see that we have transient spice models for this device but do we have any models to predict gain & phase margins such as an average model?
Part Number: TPS73801-SEP Hello;
In a space project we attend to use theTPS73801-SEP. Heat generated by the chip can be dissipated by conducting either from the top (RθJC(top) = 31.1°C/W or ψJT = 1°C/W) or bottom of the package (Rθ…
Part Number: TPS73801-SEP Hi Team,
Our customer is looking for the aging Performance (near end of life) for the device TPS73801-SEP . Can you help? do we have any aging tests for this device?
Thank you.
Regards,
Marvin
Part Number: TPS73801-SEP Hi,
In the Revision A (May 2021) datasheet, two values are specified for worst-case low level for the /EN input pin - in chapter 6.3 (recommended operating conditions) it is 0. 2 5V - in chapter 6.5 (electrical characteristics)…
Part Number: TPS73801-SEP Other Parts Discussed in Thread: TPS73801 Hi,
I'm guessing a wrong vertical axis labelling for figure 11 and 12, which makes EN-pin threshold voltage spec confusing.
By comparing TPS73801 revC and TPS73801-SEP revA datasheet…
Part Number: TPS73801-SEP HI
in the datasheet, FB pin voltage variation is about 3% over temperature range
I want to know if this applies to a single device or to a complete production batch of devices ?
if for example at 25C, the FB pin voltage of a single…