Part Number: TPS73HD3 Other Parts Discussed in Thread: TPS7A57 , TPS7A47 , Hi experts,
Can I parallel two different chips' regulator 2 output to generate a 3.3V output with double output current capability? what about the regulator 1 output, can them…
Part Number: TPS73HD3 Other Parts Discussed in Thread: LM317 Hi
My customer use TPS73HD301 to power two C2000 28374, the input voltage of both channel is 5V, and channel 1 output 1.2V, channel 2 output 3.3. Can both channels afford 750mA current load…
Part Number: TPS73HD3 Hi Sir,
Could you help to check the recommended Layout of TPS73HD301 ?
when test in high temp environment, TPS73HD301 is hot. So If I layout the "NC" pin to GND, will it be available?
there have no recommended Layout section…
Hi Nicolas,
There are several LDOs that you can use within the specs you provided. However, if you can provide more information I could provide a better solution (i.e. Iout, application of LDO).
Also, is the small package a must? There are some…