Part Number: TPS74201 Hi team,
The status of TPS74201KTWR has been changed from Last Buy to Active.
Will TPS74201KTWR continue to be available or will it be EOL in the future?
We need to manufacture our equipment for the next ten years, so please clarify…
Part Number: TPS74201 Good morning,
I have received a few weeks ago an PDN Document with ID 20230531001.3.
In this document, my P/N TPS74201KTWR appears affected, with a "Pin to Pin alternative" P/N TPS74901RGWR.
However, I think this is a mistake…
Part Number: TPS74201 Hi!
In the case where VIN is 4.2V, Vout is 3.3V, and BIAS is 5V for the TPS74201,
what would be the quiescent current in mA? Can we consider it to be around 4mA flowing through IBIAS?
Part Number: TPS74201 Good day,
Can you please advise, the datasheet shows that the VBias voltage can be up to 5V5 ? (Table 6.3)
However in table 6.5 it is stated to be Max 5.25V
The intent is to supply with 5v5 and have a output of 3V3. Thus connecting…
Part Number: TPS74201 Dear Sirs;
PLS tell me what's the differences between TPS74201RGR and TPS74201RGW? They are interchangable? I can't find the difference from the datasheet.
THX!
Donald
Part Number: TPS74201 Hello,
What is the variation curve of tps74201 output voltage and EN threshold with temperature?
What is the aging characteristic of tps74201 output voltage and EN threshold?
Part Number: TPS74201 I'm looking for the leadframe material for the TPS74201. I see the lead finish material listed on the datasheet but not the actual lead material. If someone could tell me or direct me to a material declaration document that would…
Part Number: TPS74201 Other Parts Discussed in Thread: TINA-TI Hi,
Due to the requirement I may need to control the LDO output voltage every 5mV / step.
To change the output voltage 5mV step, consider to use DAC to control the LDO FB pin to get desired…