Part Number: TPS74201 Other Parts Discussed in Thread: TPS7A52 Is this usage correct?
VOUT = 2.5V, IOUT = 1.5A
VIN = VBIAS = 3.3V
We would like to get VOUT=2.5V.
Part Number: TPS74201 Hi Team,
Would you advise my customer's inquiry below?
---
-I use TPS74201 to make 1.5V to 1.2V, but I am creating a circuit
where EN of TPS74201 turns ON earlier than VIN due to the influence of voltage sequence.
Is there a…
Part Number: TPS74201 Hello, I'm working with the part number TPS74201KTW. The absolute maximum voltage limit for this part is 6V. Is there any reliability concern operating this at a 5V +/-5% input voltage (VIN and VBIAS)?
Thanks,
Matthew Swanson …
Part Number: TPS74201 Hi, Could you inform me of TPS74201 out put discharge function? Can this device discharge the output? Customer wants to know the fall time of TPS74201 after EN low. Please tell me how to calculate the fall time. Best Regards, Yusuke / Japan…
Part Number: TPS74201 Other Parts Discussed in Thread: LP3878 Hi,
I need to know the input supply current for regulator TPS74201RGWR and LP3878MR-ADJ/NOPB and LP3878MR-ADJ/NOPB.
In data sheet it is not specified.
In order to do the board power calculation…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: TPS74201 , Dear experts,
i am trying to switch 3.3V 1A current using below circuit..(my device will run through battery so i decided to reduce battery drain time, i read data through i2c once per…
Other Parts Discussed in Thread: TPS74201 , PTH08T230W Using Vin - 2.5V, the output is adjustable between 1.0V, and 1.8V - it is possible that another supply is feeding the same rail at a higher voltage.
Question - What is the expected behavior when I apply…
Other Parts Discussed in Thread: TPS74201 Hello,
Is there a minimum load requirement for the TPS74201?
The minimum load in this circuit will probably draw less than 100mA from this regulator.
After going through the datasheet, the LDO is stable at any…
Other Parts Discussed in Thread: TPS74201 Hi All,
Now our customer evaluates TPS74201 and consider to connect BIAS pin to VIN. The datasheet recommend to connect BIAS pin to "sense point of the input supply", then I'd like to know where is the sense…
Other Parts Discussed in Thread: TPS74201 Can you please advise if the TPS74201 5x5mm QFN package can handle ~1.3W without any air flow? what would be any special layout or PCB design considerations?
Thanks
Madhuri