Other Parts Discussed in Thread: TPS74201 Hello,
My customer has aquestion about TPS74201.
Could you teach me about a question.
[Q]
In TPS74201 D/S P9 「Figure 14」,
May I have data when Cout:47uF is mounted?
Since the visitor is hurrying by Device selection…
Other Parts Discussed in Thread: TPS74201 Even if it Start Up Vin / Vbias / EN in following order, does the soft start operate normally about TPS74201? ・Vbias⇒EN⇒Vin ・EN⇒Vbias⇒Vin If the internal logic operates before Vin input, I surmised…
Other Parts Discussed in Thread: DAC3484 , TPS62420 , TPS74201 Hello experts :)
I just read the schematics of the DAC3484 Evaluation module ( http://www.ti.com/tool/dac3484evm ) There is a 6V from Connector regulated to 3.6 (3.3_LDO_IN) and 1.2 with a TPS62420…
Other Parts Discussed in Thread: TPS74201 Hello-
We use the TPS74201 device. Could you please tell us when that part was changed from being made with gold wire to copper wire?
Or has it alwyas been made with copper wire?
Did that happen when TI started assembling…
Hi
Please let me know if the IC will do the switch or transient after TPS74201 power up? Because the IP-RADIO(noise-sensitive ) signal will be interference and repeat reset.
I am having issues with slim289.tsc - the output voltage doesn't seem to be accurate. I biased the model according to the datasheet R1/R2 value, but I could never get the desired voltage output. I tried 1V, 1.2V and 1.8V -- in every case the sim outputs…
Can you please provide the following information for the TPS74201KTWRG3 part?
Junction Temperature Max (Tj Max)
Typical Power, (Pd typ)
Maximum Power (Pd max)T
Thermal Resistance Junction to Ambient (Theta JA)
Thermal Resistance Junction to Board…
Other Parts Discussed in Thread: TPS74201 Can you please provide the following information for the TPS74201KTWRG3 part?
1.Junction Temperature Max (Tj Max)
2.Typical Power, (Pd typ)
3.Maximum Power (Pd max)
4.Thermal Resistance Junction to Ambient…
Other Parts Discussed in Thread: TPS74201 My customers asks:
I interpret from the datasheet for the TPS74201, Vbias >= Vout + 1.62.
So for 1.2 Vout you need Vbias >= 2.82V and for 1.0 Vout you need Vbias >= 2.62V. If Vbias is 2.5V then Vout should…
Other Parts Discussed in Thread: TPS74201 I am using the TPS74201 LDO. I plan to possibly crowbar the input voltage. I looked through the datasheet for any information regarding what the device can handle as far as reverse currents and duration, but couldn…