Part Number: TPS745-Q1 Other Parts Discussed in Thread: TPS735-Q1 , Tool/software: Hi team,
I want to check with you if TPS745-Q1 have minimum output load requirement to achieve specified accuracy? Similar like TPS735-Q1 as below.
Thanks!
Ethan…
Part Number: TPS745-Q1 Tool/software: The RθJC(top) is greater than RθJA in the TPS745-Q1 datasheet , as follow screenshot,. It is very strange while other power regulator's RθJC(top) far less than RθJA usually. I wonder if there's a mistake of RθJC(top…
Part Number: TPS745-Q1 Tool/software: TPS745-Q1 have any simulation modeling or data about stability analysis with Bode Plot.
(1) Gain Margin
(2) Phase Margin
(3) Including temperature effect (-40C, 85C ...)
Part Number: TPS745-Q1 Tool/software: Hello
We need to have power dissipation table like of example below.
I want to calculate Tj based on the measured Tc.
Our application below.
These calculations are necessary to verify the simulation. …
Part Number: TPS745-Q1 Tool/software: Hi Team,
Harman uses the following chips in the platform, please help provide components detailed model:
1V8 LDO-TPS74501
4059465
Here is the requirement for detailed model:
Ecxml…
Part Number: TPS745-Q1 Tool/software: Hi Expert,
Have a nice day.
Could you help to explain what the V OUT(NOM) ?
What is the relationship between “VOUT = 0.95 × VOUT(NOM)” and “x1 V ≤ VOUT ≤ x2 V” (such as: “3.3 V ≤ VOUT ≤ 5.5 V” ) ?
Thanks…
Part Number: TPS745-Q1 Tool/software: Hi team,
Considering the following thread and the EN threshold vs. temp curve. I think the max value of VEN(HI) should be 1.0V not the min value is, right?
Similarly, the min value of VEN(LO) should be 0.3V not…
Part Number: TPS745-Q1 Tool/software: Hi teams,
I would like to inquire about the ramp up time of TPS745-Q1.
Will the rise time increase when the COUT increases?
Also, will the time exceed the specification in the datasheet?
Part Number: TPS745-Q1 Hi team,
Can customer test TPS74501PQWDRVRQ1 loop stability with Bode100?
Could you provide the corresponding method of loop test?
Thanks
Xiaoxiang