Part Number: TPS746-Q1 To whom it may concern,
Below is the LDO circuit in my design. However, I measure the output and it shows 3.0V instead of 2.5V.
I have a 2nd circuit with same configuration, but Vo = 1.0V. I measure it and it show 1.02V
I…
Part Number: TPS746-Q1 Tool/software: Hi team,
My customer wants to find a LDO that has adjustable output voltage. They want to control the voltage by I2C. I didn't find such device.
Is it feasible that the MCU controls the output voltage through…
Part Number: TPS746-Q1 hi, Expert
I use TPS74601PQWDRVRQ1 in my design, and I pull-up 10K resister to 3.3V .
The IN(Pin 6) is constant always on , the value is 5.7V .
if the EN(Pin 4) is low level , how about the PG status ?
I mean , if the Input…
Part Number: TPS746-Q1 Tool/software: Hello Team,
In our design we are using TPS74612PQWDRVRQ1 IC ,Can you please review the design and provide us the feedback .
Regards,
Tirthal Patel
Part Number: TPS746-Q1
Tool/software:
Please find attached schematic file for voltage regulator, this part is used for converting 5vdc to fix 3.3vdc.
I request to technical review, and let me know if any changes required.
Part Number: TPS746-Q1 Tool/software: Dear TI experts,
My customer made their first schematic using TPS74601PQWDRBRQ1. Could you review this schematic?
Best regards,
Chase
Part Number: TPS746-Q1 Tool/software: Hi Team,
May you help verify the startup time of TPS746-Q1? The result shows 1.17ms which is higher than datasheet shows. Our Cout is also 1uF.
Roy
Part Number: TPS746-Q1 Other Parts Discussed in Thread: TPS764 Tool/software: Hello, The TPS746-Q1 has many options, but the datasheet doesn't inform how to order the correct part number. For example: TPS74650PQWDRBRQ1 I suppose that is the 5V fixed output…
Part Number: TPS746-Q1 Tool/software: I am wanting to perform a resistance measurement between the output of the TPS746-Q1 and ground to verify that there are no shorts before turning on power. The block diagram shows 2 internal resistors in series between…