Part Number: TPS74701-Q1 Other Parts Discussed in Thread: LM65645 , LM5137 Dear Team We need support for selecting LDOs for following.
3.3 V to 40 V for 3.3V@ 2A-3A. DC-DC
Vin 6V for 1.8V @300mA LDO from 3.3V supply
Vin6V for 1.2V @500mA. LDO…
Part Number: TPS74701-Q1 Hi TI Team, Could you suggest me a Low Noise high PSRR LDO capable of providing Output voltage range of 3v to 3.8v @500mA, Input voltage is 5v. This is for a carrier board of Nvidia SoM for the automotive application.
Part Number: TPS74701-Q1 Tool/software: Dear Texas Instruments Support Team,
I am currently performing a signal integrity analysis and require the IBIS model for TPS74701-Q1 . However, I was unable to locate it on the product page or TI’s model repository…
Part Number: TPS74701-Q1 Other Parts Discussed in Thread: TPS74701 Tool/software: Dear Texas Instruments Support Team,
Hello,
I have downloaded the PSpice average model for the TPS74701-Q1 (part number TPS74701QDRCRQ1) from the TI product page. However…
Part Number: TPS74701-Q1 Other Parts Discussed in Thread: TPS74701 Tool/software: Hello,
I am simulating the TPS74701 LDO in PSpice and noticed that the soft-start (SS) pin voltage initially rises to approximately 39.63 V . According to the datasheet…
Part Number: TPS74701-Q1 Tool/software: Hi TI Expert,
Could you teach me how to calculate the actual output based on following condition after considering following parameter?
Scenario 1:
VIN: 3.3V
VOUT: 1.2V
VBIAS: 5V
IOUT: 250mA
…
Part Number: TPS74701-Q1 Other Parts Discussed in Thread: TPS74701 Hi Expert,
According to TPS74701 datasheet,when Css open, minimum start-up time is 200us,This start-up time is from EN high to output begin to rise, right?
Besides,when Css open…
Part Number: TPS74701-Q1 Other Parts Discussed in Thread: TPS74701 Hi, Expert,
TPS74701 is used in my application to output about 1V2/220mA as second level power LDO. Input voltage is 3V3. Unfortunately, there are some board with PIN10 floating(not…
Part Number: TPS74701-Q1 HI Team,
Can you please check what the Vdo(max) @300mA over-temperature is for the TPS74701-Q1? This is only defined at 500mA in the datasheet.
Thanks, Mitchell