Part Number: TPS74801-Q1 Hi TI team Please help to review the below schematics of TPS74801-Q1
Input Voltage : 5V Output Voltage : 3.3V Output Current : 0.5A
Part Number: TPS74801-Q1 Hi TI Team,
We are evaluating the TPS74801-Q1 for the following operating condition:
VIN = 1.3 V
VOUT = 1.2 V
VBIAS = 3.3 V
Peak load current = 1 A
Maximum ambient temperature = 85°C
While reviewing the datasheet…
Part Number: TPS74801 Hi Team,
Will the OCP be triggered on the TPS74801 before VOUT reaches 0.8VOUT?
We have a 3.3V VOUT line. The inrush current reaches 2.6A during power-on (VOUT=0.257A).
We want to confirm whether this will trigger the OCP.…
Part Number: TPS74801 Team,
Customer found the failure in the manufacuring site. Could you hlep with this issue and refer to the link for more details. thanks.
TPS74801_TI_Inquiry.pdf
Part Number: TPS74801 Hello,
I am using the standard TPS74801 resistor configuration for 3.3V output, 3k57 and 1k15. I have an input voltage of 3.69V and output current <400mA. The output voltage is 2.69V. Looking back at Vref, I see that it is 0.657V…
Part Number: TPS74801 Hi Team,
The DS shows that the EN pin input level minimum value is 1.1V, but customer measured 0.8V on their board, and I measured 0.88V on the EVM.
I saw there is the thread that the DS value is for customer to do the design…
Part Number: TPS74801 There are two regulator markings.
Good : BTO 2CI AJCE
Bad : BTO 488 C9ZK
Pin G1 (the belly) and 6 are shown on the schematic as GND. Internally, however, they are not connected. Pins 9 and 10 are internally connected.
On…
Part Number: TPS74801 Hi experts
Hope this finds you well.
Regarding the TPS74801 datasheet (SBVS074N – JANUARY 2007 – REVISED JUNE 2024),
VOUT: Output voltage range in section 5.5 Electrical Characteristics is listed as (min)VREF to (max)3.6V,…