Part Number: TPS74801-Q1 I need to do Monte Carlo Tolerance analysis for this MPN. Can you please suggest simulation tool for that ? Also I am unable to get spice model for this MPN .Can you please provide spice model for same
Part Number: TPS74801 Other Parts Discussed in Thread: TPS54620 Hello,
The two tps74801 in the following figure are not working properly. All output is about 1.0V.
3.3V is right. PG_1V2 is 1.8V.
Why they are working abnormally? Thanks!
Part Number: TPS74801 Hi,
Will it make any difference if I place the voltage divider connected to the Feedback after the capacitor (noise reduction)?
Regards,
Jeevan
Part Number: TPS74801 Hi,
In the application circuit of TPS7481, PG is connected to Vout as shown in the image
Whereas in the layout recommendation, PG is connected to VCC.
Which one needs to be followed? In our application, we have fixed the Vout to…
Part Number: TPS74801 Hi,
In datasheet of TPS748, condition of typical characteristic with VBIAS=5V for testing. However, figure 6-17 which show current limit curves illustrates relationship between ICL and (VBIAS-VOUT), and Vout = 0.8V is noted at chart…
Part Number: TPS74801 Hi,
Could you please provide the max and min value of Iss, customer is using 3300pF as soft start Cap design but the test result slew rate is not accuracy, we need the max and min value to evaluation.
Part Number: TPS74801-Q1 Other Parts Discussed in Thread: TPS74801 Hi Team,
May I know whether we have PSpice model for TPS74801-Q1?
Or we should directly use the PSpice model of TPS74801.
Is there any difference between them?
Looking forward to your…
Part Number: TPS74801 Dear Team,
The VDO requirements of the TPS74801 specification are shown in the figure below. According to the connection method in our schematic diagram, VIN=Vbias=3.3V, can it output a voltage of 2.5V? Our current application dropout…