Part Number: TPS74901 Other Parts Discussed in Thread: TPS74801 , TPS7A53 Hi team,
Can you advise me on an alternative part as RT5793? P2P solution? It's 3A LDO, and I cannot find one at TI.
only TPS74801 1.5A, TPS74901 2A
and suggestion?
Part Number: TPS74901 Hi team,
My customer use our LDO TPS74901 to realize the input=3.8V and output 3.3V/2A. Attached file is SCH.
I am not sure how to configure TPS74901 Vbias. It said Vbias need >1.75+ Vout in the datasheet.
Could you help me review…
Part Number: TPS74901 Other Parts Discussed in Thread: TINA-TI Hello support team,
I ran a transient analysis simulation of TPS74901. I used "slim257.tsc" which is downloaded from "TINA-TI Transient Reference Design" on your homepage of TPS74901.…
Part Number: TPS74901 Other Parts Discussed in Thread: LP38503-ADJ , TPS7A84A , TPS7A53 Hi,
which alternative would you recommend against LD39300?
Package may be differ.
Let me know if you can recommend any with these few pieces of information ,
Thanks
…
Part Number: TPS74901 Other Parts Discussed in Thread: TPS740 Hi,
I am using the TPS74091 to generate 1.8V from 2.5V. Can I connect Vbias to the same 2.5V as Vin? Or it has to be 1.75V larger than 1.8V?
Thank you.
Part Number: TPS74901 Hi Team,
My customer is using TPS74901 and seeing some output voltage ringing during transient when they are using 609uF output cap, but did not see the ringing at 309uF output cap.
I did a simulation using the Tina reference design…
Part Number: TPS74901 Hello,
My customer would like to use TPS74901KTWR.
They are asking if this device have overvoltage/undervoltage protection function for Vin and Vout.
Could you kindly tell me the answer, please?
Best regards,
K.Hirano
Part Number: TPS74901 Other Parts Discussed in Thread: TPS74801 Dear Sir,
Customer design TPS74801 for previous projects but the requirement increase to 3A. Could TPS74901 support 3A application?
TPS74901 is same package as TPS74801. Is there any difference…