Part Number: TPS75003-EP Other Parts Discussed in Thread: LMH5401-SP Hi Team,
I don't find any radiation information about TPS75003-EP, only latch-up, can you please advise?
Thanks,
Shlomi
Part Number: TPS75003 Hi:
When customers use TPS75003 as the power supply of the FPGA, the output current is 3A, SOT-23 is needed, and the Id current exceeds 3A PMOS. Recently, it was found that the external PMOS SI2323DS-T1-E3 recommended by TI has…
Part Number: TPS75003 Hi,
Please refer to the attached (or pasted) portion of the schematic below. I am using this TPS75003 to provide power to a Xilinx FPGA, a Virtex. I am getting this information second hand, so I apologize in advance. I am told that…
Part Number: TPS75003 Hi,
Could you tell me about LDO of TPS75003.
If not use LDO,How should I connect each pin?
I think that it is as follows.
VIN3:GND
OUT3:Open
EN3:GND
FB3:GND
SS3:GND
Is this correct?
Best Regards,
Yuto Sakai
Other Parts Discussed in Thread: TPS75003 Hi,
I have designed a power circuit using the TPS75003 chip in order to power FPGAs and ADCs on a data acquisition board.
The problem is that I am observing that the linear regulator output (OUT3) is working differently…
Other Parts Discussed in Thread: TPS75003 Hello,
I am having trouble with EN3 pin on TPS75003. According to the datasheet the minimum threshold to turn on the LDO at the EN3 pin is 1.14V. However, I have found multiple devices turn on at 0.90V. Is there…
Other Parts Discussed in Thread: TPS75003 Hello,
I am currently using TPS75003 IC in one of my designs using. SPARTAN 3 FPGA. The schematic is attached.
Iam not seeing any switching waveforms at the gate of either Q2 or Q1. I am seeing a continuous DC…
Other Parts Discussed in Thread: TPS75003 , CSD25211W1015 Hello everybody!
I'm having troubles with the TPS75003. I've to feed a Spartan 6 LX150, that requires 2A on the 2.5V output.
Obviously, the component should not be suitable since has a maximum…
Other Parts Discussed in Thread: TPS75003
Hi,
I'm thinking about
using the TI TPS75003 to provide the core and I/O voltages for an
Altera Cyclone II FPGA (2C5 type) and a PIC microcontroller
(PIC18F85J50). Essentially, I'm looking at a modified implementation…