Part Number: TPS763 Hi,
What is the output impedance of the TPS763 when EN is low or Vin is low (in my application both are tied together). Would it be the same as the output impedance in dropout?
Thanks,
JMMN
Part Number: TPS763 Hi TEAM,
We read the datasheet of TPS763-Q1, but the input current of EN pin is -0.5uA maximum in Page 5. What I don't understand is
1) Why is the current negative
2) Why is the current is negative no matter the EN is connected…
Part Number: TPS763-Q1 Other Parts Discussed in Thread: TLV702-Q1
Hi,
Currently I got a question from customer that TPS763-Q1 datasheet mentioned 0.3-10 ESR is needed for a 4.7uF Output capacitor. I checked our part with Rohm's BU33SD2MG(currently on…
Part Number: TPS763-Q1 Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 Hi team
customer wants Vout = 5.7V at Max Iout 80mA with Vout deviation = +- 3.5%.
he will use TPS76301-Q1 for adjustable Vout.
D/S says Vout deviation = +- 3% for 5V <= Vout…
Part Number: TPS763 Other Parts Discussed in Thread: TPS709 Hi. I wanted to make design same like in TIDU298 , but what seemed strange for me is that in this application note the input voltage of TPS76333DBVT is shown as 5-12V.
But at the same time in TPS76333DBVT…
Part Number: TPS763 Hello,
We’re wondering how best to calculate the accuracy of the adjustable version of the TPS76301.
Page 4 of the datasheet shows 0.97x Vout to 1.03x Vout. Does this already take into account accuracy of the set resistors? Or…
Part Number: TPS763 Hello,
I was looking for the output voltage range of the TPS76325 (5V). There are tow sources in the datasheet ( http://www.ti.com/lit/ds/symlink/tps763.pdf ). The problem is that these sources do not agree on the output range...
The…
Part Number: TPS763 Hi team,
I noted this part has a current limit level of >0.5A, while it is only specified at up to 150mA. I do not why. My customer's ckt drinks only tens of mA in most of operating time. But in some very short duration they need up…
Other Parts Discussed in Thread: TPS763 Hi,
Based on TPS763 datasheet, ESR stable region is between 0.3 to 10 Ohm (for instance, ESR curve in Figure 18).
How to determine or verify whether the regulator is stable or not?
Should I check whether the output…
Part Number: LP2985 Other Parts Discussed in Thread: TPS763 Hello,
My customer is trying to drop LP2985-50DBVR into their existing schematic below with no board changes because of supply issues with TPS763.
Specs:
Vin can be as low as 6.4V.
We planned…