Part Number: TPS766 Tool/software: hi TI,
In the spec of TPS76601DR "legacy chip" and "new chip" spec.
If my customer orders now, we will ship "new chip" part or "legacy chip"?
Part Number: TPS766 Hi TI team,
Recently we received TI device TPS76633DR,the marking has great difference compare with device we received before,could you please provide PCN file for the change?
Part Number: TPS766 Hi Team,
Is it possible to connect the PG and NC/FB pin directly to the GND if customer don't use PG function? From the block diagram it seems okay for this case, would like to double check with you, thank you.
Sincerely
…
Part Number: TPS766
Hi,
My customer is facing a problem when using TPS76633, when turned off there is a reverse on output voltage and we can not explain why it occurs. The schematic and the waveform of Vout are showed as below, upper green line is…
Part Number: TPS766 Hi,
I was going through the Datasheet, and we see a load transient of ~200mV w/ CL=4.7uF when IOUT=0 to IOUT=250mA.
Do we know what will be the slew/transient rate? Scales on the graphs are not clear, can you please let us…
Hi Antonio,
Thank you for the information. The low-active enable (shutdown) function is not a common feature we have on our LDOs.
Unfortunately I was not able to find one in SOT-23 package. Here are some devices that do have this feature: TPS766,…
Hi Jamie,
TPS766 can supply 250mA; however, the LDO does not sink current.
My intention was to point out that the voltage appears to be biased higher than the regulated 3.3V for most of your scope shot. The low point of 3.3V is the only point on the…
The TPS766xx data sheet includes some typos concerning output capacitance. Please reitterate the Cout requirements and in particular comment on the ESR requirement for larger capacitors. It appears from the data sheet curves that the requirement is really…