Hi Edgar,
Thanks for your help. some more questions may need your help.
1, I noticed that the Vref range of TPS73HD301PWPR is 1.147~1.217 within whole temp range -40~125°C. But in 25°C, there’s only typical value 1.182V. Do we have the data of the part…
Part Number: TPS767-Q1 Other Parts Discussed in Thread: DS90UB921-Q1EVM , TLV840-Q1 , TPS767 Hi Expert,
I see TPS767D318PWP is used for supplying DS90UB921AS-Q1 in its reference design. You can see the TPS767D318PWP part as below. As required, the 3.3V cannot…
Part Number: TPS767 Hi,
is the part MLA00340PWPR identical with TPS76750QPWPR?
My customer has both part numbers is their system and wondering if there are any differences between these two.
Thanks and regards,
Alen
Part Number: TPS767 Hi Team,
One of our customer was using the TPS767 (5V variant) for their design and they're encountering intermittent problems where noise was being introduced into the system that was traced back to the TPS767. The datasheet recommends…
Part Number: TPS767 Other Parts Discussed in Thread: TLV767 , TPS768 Hi Team,
Do you have any pin-to-pin device for TPS76733 both from performance and cost aspects?
Application is 5V to 3.3V, 1A load, need enable pin and SOIC-8 package.
Best Regards, …
Part Number: TPS767-Q1 Dear team,
My customer used this device in their system, and the condition is Vin=5V, Vout=3.3V, Iout=500mA. When they test this device's surface temperature with thermocouple under 75°C high ambient temperature, they found that…
Part Number: TPS777 Other Parts Discussed in Thread: TPS775 , TPS767 Tool/software: Would you let me know about Min and Max value for RESET time-out delay?
Datasheet is described only Typ value: 200ms.
Best regards,
Satoshi
Part Number: TPS767 We want to know the history that the material content of bond wire was changed from gold wire to copper wire.When the change happened?Was there a PCN document?How many TI part number happened the change?Would you provide the PCN document…
Part Number: TPS767 Hi team,
I have a question about TPS76701. If the output voltage of TPS76701 is set to 5V by external resistors,will the dropout voltage be same as TPS76750?
Best regards, Tsuyoshi Tokumoto