Part Number: TPS782 Hi, in error I have only grounded pin 3 and the thermal pad for this part, but failed to ground pin 5. This is causing the regulator to produce 2.2V instead 1.8V. I currently have the VDDIO pin of a DS90UB925 connected to this regulator…
Part Number: TPS782 Other Parts Discussed in Thread: TPS61222 , TPS7A03 , TPS7A02 Hi, Support Team
A circuit was formed by combining the TPS78230 and TPS61222.
However, a problem has occurred, so we will contact you as follows.
First of all, please…
Part Number: TPS782 I designed in the 2.5, 3.0, and 3.3 V versions of this regulator without noticing the awful load transient response (fig 19 in the data sheet). This has become a problem in the prototype. Is there a drop-in replacement for this family…
Part Number: TPS782 Can I put two TPS78230DDC regulators in parallel? They would be controlled via the ENables. Only one will be on at any time, although, it may be possible that both are enabled momentarily while switching ENables.
Part Number: TPS782 What happens to the output of the LDO TPS 78233 when the input voltage is lower than the regulator output voltage 3.3 V? For example, when the input voltage is 2.5 V, how many VOUT voltages and What is the current limit at that time…
Part Number: TPS782 hi,
on TPS782 datasheet, bottom of page 12 it is stated "The TPS782 series is designed to be stable with standard ceramic capacitors with values of 1.0 μF or larger at the output."
I have been always puzzled by such sentences,…
Part Number: TPS782 Other Parts Discussed in Thread: TPS7A05 Hi Sir,
I want to find a LDO to replace TCR3UM30A (TOSHIBA), it's quiescent current is 0.38uA(Typ.).
The TPS782 is 0.5uA, has any device could meet or better this spec.? the size is smallest…
Part Number: TPS782 Other Parts Discussed in Thread: TPS3780 Hi all, I have a TPS78233DDCR with Cin=1uF and Cout = 1uF, both X5R; EN pin always enabled. When Vin<3.6V, the output voltage is equal to Vin (LDO is in "Operating Mode Droput", page 11 of datasheet…
Part Number: TPS782
Hi Team, Could you please review the XC6206-33 spec and propose the alt. solution to replace? SOT23-3 is the prefer package www.torexsemi.com/.../XC6206.pdf
BR, SHH