Part Number: TPS798-Q1 I am working on TPS798-Q1 LDO design for following requirements:
Vin- 6 to 36V (42V transient)
Vout-3.3V
Iout- 5mA
Temperature req- -40 to 85
Application- Wakeup Supply
In my schematic I have connected 1R resistor in…
Part Number: TPS798-Q1 Other Parts Discussed in Thread: MSP430FR2476 Tool/software: Dear Experts,
I have some questions regarding the “IEEE 802.3cg 10BASE-T1L Power over Data Lines Powered Device Design” Application Note:
LDO Usage for 3.3V Supply…
Part Number: TPS798-Q1 Tool/software: Hi,
I want to use 180uF capacitor on the output. Will I have a problem with stability?
I will also have a smaller low ESR cap as recommended by the datasheet too.
Part Number: TPS798-Q1
For item: TPS79801QDGNRQ1
Here I just wonder: why this part has four abnormal solder pad on the back board, we concern this will affect planarity, and soldered lead reliability or even solder shorts, would you please kindly…
Part Number: TPS798-Q1 Tool/software: Hi team,
What is the influence if we add 460pF between FB and GND? And what is the relationship between the cap value and influence? Thanks!
BR
Jiawei
Part Number: TPS798-Q1 Hi TI Experts!
I have this part with different coatings on top and bottom leads. The top coating is golden. May I know if this is normal in manufacturing? If yes, why?
Part Number: TPS798-Q1 Hi Team,
For the IFB spec in the datasheet, is the 0.2uA Max spec across full temp, or is that entire line item only pertinent to 25C?
Is there any data for this spec at higher VIN?
Thank you,
Jared
Part Number: TPS798-Q1
Hello.
There are 3 NC pins on TPS79801QDGNRQ1 device. I can see in datasheet that there is no internal connections to these pins, but I can't find a certain description on how this pins may be handled.
So I'm asking for support…