Part Number: TPS799 Im using TPS79928 fixed LDO which has 3.3V input and 1.8V enable. I'm getting output pulse of 540mV when the 3.3V input reaches 1.2V level but EN is still low. Could you please clarify the issue why the output is toggling to the intermediate…
Part Number: TPS799 I'm using the TPS79928 fixed LDO which has 3.3v input and 1.8V enable signal. When the EN is low and input voltage reached 1.24V the output has a pulse of 0.54V and stays there untill enable is high. I want to know the reason for the…
Part Number: TPS799-Q1 Tool/software: Hello,
I have downloaded the PSpice average model for the TPS799-Q1 (part number TPS79918QDDCRQ1) from the TI product page. However, the .LIB file contains $CDNENCSTART encryption blocks, and my simulation tool…
Part Number: TPS799 Tool/software: Hello,
I have part TPS79912DDCR fixed voltage 1.2V and for some reason its output is 0.6V. This problem only happens with new ICs with top markings CCF _ _ _. When I use an IC with top markings "1127P" it works fine…
Part Number: TPS799
Tool/software:
Hi,
The datasheet of TPS799 says Vdo drops while Vin increase, could you help explain why?
For PMOS,
i think if Vin increase, and Iout fixed, then -Vds increase. Then -Id increase slightly. so in order to keep…
Part Number: TPS799 Tool/software: The TPS799 accepts a bypass cap on the NR pin to reduce noise. How does one determine the capacitance value and type?
Marcus
Part Number: TPS799 Tool/software: Hello,
Can you please send us a certificate of compliance to IEC62368 or IEC61010 or other standard (about electrical security) for TPS 79933 ?
Part Number: TPS799 Hello,
I have a few questions about TPS79901, the adjustable-voltage version of the TPS799 family.
The section 8.2.2.1 Input and Output Capacitor Requirements of the data sheet says, "The TPS799 is designed to be stable with…