Part Number: TPS799 Hello,
The output is volatge is rated up to 6.5V, the discharge resistor is 400Ohms. In an application with high output capacitance, without load, the capacitor's energy will dissipate in the discharge resistor
Is there a power…
Part Number: TPS799 Dear Team, We are using TI's TPS79933DRVT LDO in one of designs. We just want to know the minimum voltage rating needed for the noise-reduction capacitor (CNR) which will be connected to pin 'NR'. Whether it just has to bypass the max…
Part Number: TPS799 I have designed my board with the TPS79933 on board. I have built about 500 without issue.
I have since outsourced the assembly and now the TPS79933 have a 60% failure rate. They are giving me 1.2-1.8v output instead of 3.3v.
What…
Part Number: TPS799 Hi,
my customer would like to use the TPS799 ( TPS79915 variant ) in their new project and would like to know what the load transient response is going to look like under the following conditions: Vin = 5V, Vout = 1.5V and load varies…
Part Number: TPS799 Your MTBF/FIT Estimator only shows FITs @ 60% confidence level.
Please send me reliability data (FIT or MTTF) @ 90% confidence level for the device TPS79925DDC. Thank you in advance. Regards Axel
Part Number: TPS799 The TPS79901 version of the IC is able to be used in the following application:
Vin = 5V
Vout = 1.8V
Iout = 200mA
WEBENCH is able to produce this application.
But if I use the TPS79918 (fixed version of the part), WEBENCH states that…
Part Number: TPS799 Hi,
My customer is using TPS79901. He has issue big inrush current at start-up. Peak current value is about 2.57A. He has questions below.
Q1: What is "Inrush Current Protection with EN Toggle" in datasheet ? Could you let…
Part Number: TPS799-Q1 I would like to confirm the cause of the unexpected output in EN low for TPS799-Q1.
I attached the waveform.
The conditon is VIN = 3.3V, EN = 2.7V, input capacitor 4.7uF and output capacitor 2.2uF.
The output voltage in EN low…