Part Number: TPS7A02 Other Parts Discussed in Thread: INA333 , , TPS783 , TPS7E81 I have the TPS7A02 (1.2V) fed into the vref of the ina333. This works great until the ina 333 output goes higher than 1.2V. Then the LDO jumps from 1.2V to 1.29V. I can…
Part Number: TPS7A02 Hi
TPS7A0212PDBVR & TPS7A0312DQNR If these are to be used on the Intel Nova Lake-BGA platform, could you please advise which of these two is more suitable for this platform? (Why?)
Thanks
Part Number: TPS7A02 Other Parts Discussed in Thread: TPS7A11 Tool/software: Hi Team
could TPS7A02 support Vin 2.1 and Vout 1.8 when I out=200mA?
or do you have any recommendation support such low drop out?
BRs
Brian
Part Number: TPS7A02
Application: TPS7A0230PDQNR in a battery powered device.
We get thousands of product returns of this device from customers. On each returned device the LDO is frozen in disabled mode.
There is 4.0V Vin, 0V Vout, and 3.6V on…
Part Number: TPS7A02
Tool/software:
Hello;
I want to use TPS7A0233 for super capacitor Load. I will use a diode at Output to stop current flowing from output to input of LDO. However datasheet mentions that Maximum Load capacitance for this I.C…
Part Number: TPS7A02 Hello,
How will TPS7A02 handle inrush current if connected to large output capacitor 220uF.
Input voltage is 4.0V .
I was not able to run Pspice for this condition.
Thank you
Part Number: TPS7A02 Hi,
We have used a TPS7A0233 in one our products that is supplied by a Li-ion battery. The whole board is supplied by this LDO which is always ON, and there is no other parts on Vbat line. The overall current consumption in shutdown…