Part Number: TPS7A03
Tool/software:
So I tried testing stand alone IC TPS7A0330PDBVR on my bare PCB to see the Quiescent current without any load at the LDO output. When I supplied 4.2V at the input the current consumption was showing 6mA which is…
Part Number: TPS7A03 Tool/software: Hi Team
Could you help provide me the maximum enable pin leakage current value of TPS7A0318 & TPS7A0218?
Does the Ven level impact on enable pin leakage current value?
If no impact, the leakage current will…
Part Number: TPS7A03 Other Parts Discussed in Thread: STRIKE Tool/software: Hi team,
My customer test their product ESD ability with 15kV, after the test they find TPS7A0328 has no output.
Removed the IC and soldered to another board and found that…
Part Number: TPS7A03 Tool/software: Hi team,
Customer is evaluating TPS7A0318 in their application.
They get one condition which input is 1.85V, and max output current is 90mA.
Based on the waveform, the drop out voltage at 1.8V/90mA would be…
Part Number: TPS7A03 Hi,
I am using TPS7A0333DBVR LDO in my circuit, could you please provide the spice model of this part ? So that i can perform TINA simulation.
Regards
Shubham
Part Number: TPS7A03 Hi
We have received two kinds of marking for this product, one is G4 and the other is P5. According to the datasheet, it is G4. Could you please help confirm if P5's marking is correct? thank you.