Part Number: TPS7A11 Hi team,
Csutomer is evaluating TPS7A1112DRVR in their project. Could you help check two quiescent current specs on the TPS7A1112DRVR for a radar power application?
Application conditions:
- Vbias: 3.3V / 2.1V / 1.8V
- Vin…
Part Number: TPS7A11 Hello team,
I am in need of information on the UBM (Under Ball Metallization)/SRO (Solder Resist Opening) of this device TPS7A1118PYKAR.
Thank you,
Austin Allen
Part Number: TPS7A11 Other Parts Discussed in Thread: TPS7A21 Hi support,
I would like to use TPS7A1118PDRVR to power the nrf52840. The input voltage is a battery voltage from 1,5 to 5,5 V. I use LTC3536 DC-DC regulator to step-down the voltage to 3…
Part Number: TPS7A11 In the recommended circuit of TPS7A1108, the VIN VOUT is 0.2V, but it is suggested to be greater than 0.5V. Is this a contradiction or other issue? Could you please help to answer it?
Part Number: TPS7A11 Hi Experts, Good day. Does the current limit circuit here provides overcurrent protection also or just short-circuit protection? I believed that the current limits circuit is protecting against overcurrent faults too other than the…
Part Number: TPS7A11 Other Parts Discussed in Thread: TPS74801 One or the most typical method to design a suitable PDN is the target impedance method. The datasheet does not contain any graph/chart related to impedance output.
It is indeed possible…
Part Number: TPS7A11 Hello Support Team,
Customer inquires how to measure temperature and assume junction temperature when they use TPS7A11 with heat sink on top of IC, could you support? Referring SPRA953 application note, Psi-JT can't be used in…
Part Number: TPS7A11 Hello all,
I am using the TPS7A1118 to provide1.8V with the following set up, to supply an ADC:
-Vin = 3.3V
-Vbias = 3.3V
-EN = 3.3V (all 3 pins are tied to 3.3V power plane)
-The NC pin is not connected, and GND pin tied…
Part Number: TPS7A11 Other Parts Discussed in Thread: TPS74701 Hi Team,
I have received the TPS7A1110 P DRVT part. The P denotes that the active discharge circuit is enabled. Looking at the ordering info of the TPS7A11 parts, it seems that it is only…