Part Number: TPS7A16-Q1 Hi, TI Team:
when we used TPS7A1633QDGNRQ1 to convert 12V to 3.3V, and found the output(VCC_RTC_3V3) current is only 10uA, but TPS7A1633QDGNRQ1 itself (test on D5100) used 270uA.
Could you tell me how big comsuption current…
Part Number: TPS7A16-Q1 Hi Team,
Here is a problem we found when developing TPS7A1601QDGNRQ1.
Customer designed with a wrong schematic, they didn't connected the DELAY pin as the datasheet recommended, but connected like this schematic. Which lead…
Part Number: TPS7A16-Q1 Tool/software: When doing JumpStart experiment, TPS7A16-Q1 will burn from 0V to 48V, the phenomenon is 5V output to ground impedance 150Ω, Delay pin to ground impedance 0Ω. There is no relationship between Delay and Vin found in…
Part Number: TPS7A16-Q1 Tool/software: Hello
I like to continue with the PSpice model issue for TPSA16-Q1. When adding shunt transient protection diodes on the input such as TVS diodes such as SMBJ33CA the PSpice model cannot converge?
Part Number: TPS7A16-Q1 Other Parts Discussed in Thread: LM74930-Q1 , LM74930 , Tool/software:
Hello,
I am using TPS7A1633QDGNRQ1 in the low current circuit, among other functions, to provide a ON/OFF functionality for Ideal diode surge stopper LM74930…
Part Number: TPS7A16-Q1 Tool/software: Hello,
A related question to the device PG pin current is the maximum current that the device may sink without reliability issues (regardless of the actual voltage output - no curves)
The absolute maximum rating…
Part Number: TPS7A16-Q1 Tool/software: Hi expert,
My customers noticed there are 2 version of package info in the 7A16-Q1's datasheet. which one should they refer to when drawing the PCB? Any reasons for have two example layouts?
BR,
Manu
Part Number: TPS7A16-Q1 Tool/software: Hello,
In the datasheet, the TYP value for load regulation and line regulation is 1%, but can you tell me the MIN and MAX values?
Thanks!
Part Number: TPS7A16 Hi Folks,
I have a question related to the footprint that actually have in my design for the TPS7A1650QDGNRQ1.
In the footprint the central pad for dissipated the heat is like a hatched (see the picture)
In the datasheet…