Part Number: TPS7A16-Q1 Tool/software: When doing JumpStart experiment, TPS7A16-Q1 will burn from 0V to 48V, the phenomenon is 5V output to ground impedance 150Ω, Delay pin to ground impedance 0Ω. There is no relationship between Delay and Vin found…
Part Number: TPS7A16-Q1 Tool/software: Hello,
A related question to the device PG pin current is the maximum current that the device may sink without reliability issues (regardless of the actual voltage output - no curves)
The absolute maximum rating…
Part Number: TPS7A16-Q1 Tool/software: Hello,
In the datasheet, the TYP value for load regulation and line regulation is 1%, but can you tell me the MIN and MAX values?
Thanks!
Part Number: TPS7A16-Q1 Hello,
I am simulating this device (TPS7A1633-Q1), and I was expecting to see a output of 3.3V. according specs.
https://www.ti.com/product/TPS7A16-Q1?keyMatch=TPS7A16-Q1&tisearch=search-everything&usecase=GPN#design-tools-si…
Hello Shyama,
Many thanks for your question!
Since your Vi - Vo is greater than the Absolute maximum of the device as per the LM317 datasheet, it may cause permanent damage to the device. Exposure to absolute-maximum- rated conditions for extended periods…
Part Number: TPS7A16-Q1 Hi team,
For TPS7A16-Q1, there are two package drawings, DGN0008C and DGN0008B - which package drawing the device is using? I notice the thermal pads in the two drawings are different in size.
Part Number: TPS7A16-Q1 Other Parts Discussed in Thread: TPS7A16 Hi experts
Do TPS7A16-Q1 and TPS7A16 use the same die?
My customer is having availability issues with TPS7A16-Q1 and is considering substituting the non-Q1 part.
Thanks!
Jim B