Other Parts Discussed in Thread: TPS7A16-Q1 1. The input of TPS7A16-Q1 chip is 3V to 60V. Can this chip receive negative voltage output?
2. If not, please help me find an LDO with a negative voltage and output -12V?
3. If not, please help me find a chip…
Part Number: TPS7A16-Q1 Hi team,
TPS7A1650. VIN and EN are connected together, PG is connect to GND.
We find when VIN rise to 3-5V, which will result a output <5V. During these period, the Iq is 20-30uA. When VIN rise to a larger voltage, like 12V, Iq…
Part Number: TPS7A16 Hi team,
I'd like to confirm the ESD protection schematics of TPS7A1633-Q1. It's need for how the voltage sneak to another pins inside the TPS7A1633-Q1.
Could you tell me the schematics of ESD protection?
Regards,
Nishimu…
Hello,
TPS7A16 A -Q1 was released after the TPS7A16-Q1 with improved functionality. The specifications are the same but the A version is better behaved.
Regards,
Nick
Hi Dice-K,
TPS7A16A is a spin from TPS7A16A and there are some differences for the EN Voltage requirements and UVLO
TPS7A16A EN pin:
Compared to TPS7A16:
Also, notice the recommended slew rate for TPS7A16A. This question has been addressed several…
Part Number: TPS7A16A-Q1 Other Parts Discussed in Thread: TPS7A16 Hi experts,
May I know what is the different between TPS7A16 01 AQDGNRQ1&TPS7A16 33 AQDGNRQ1&TPS7A16 50 AQDGNRQ1?
Thank you.
BR,
Aaron Chen
Hi Sepeedah,
TPS7A49 DRB could fit on the TPS7A16 pad. The power pad on the TPS7A49 is a little smaller than the TPS7A16 and the leads go the same distance from the edge of the package inwards, so there would be extra room to ensure there's no pin shorting…
Part Number: TPS7A16A-Q1 Other Parts Discussed in Thread: TPS7A16 Hi team,
My customer thinks to use TPS7A16A-Q1 48V to 12V regulator.
Load current is less than 10mA, but concerns about inrush current into output cap when device initially power-up.
This…
Part Number: TPS7A16A-Q1 Other Parts Discussed in Thread: TPS7A16-Q1 , TPS7A16 In another post, it was stated:
"While rare, TPS7A16-Q1 can experience issues in applications where the EN slew rate is faster than 1.5 V/us (note that our maximum recommended…
Other Parts Discussed in Thread: TPS7A16-Q1 Hi team,
May I know TI's LDO has fully protection for output short circuit? In my case, we need 24VDC convert to 12VDC / 60mA for ouput spec and wide input rang up to 60VDC for load dump.
Looks TPS7A16-Q1…