Hello Ethan
Thanks you comment.
It is difficult working FET swap test due to drain pad and via.. also I don't have AON6226. For debugging I will board revision.
- add bootstrap diode : " V1FM10-M3/H" is applied EV kit already. (Low Vf)
-…
Part Number: TPS7A16A-Q1 Other Parts Discussed in Thread: TPS7A16-Q1 , TPS7A16 In another post, it was stated:
"While rare, TPS7A16-Q1 can experience issues in applications where the EN slew rate is faster than 1.5 V/us (note that our maximum recommended…
Part Number: TPS7A16A-Q1 Dears,
I want to know about the difference between TPS7A1650-Q1 and TPS7A1650 A -Q1? could you tell me? thanks. it's better to provide relative files if you have.thanks.
Part Number: TPS7A16A-Q1 hi Team,
does TI have similar parts to the maq5281? DS available online
key features
input 6~120V
automotive qualify
consumption 6uA
Thanks
Part Number: TPS7A16A-Q1 Hi Team,
When using the TPS7A1601A-Q1, should an RC filter be implemented between the driving source and the EN pin?
Some regulators require an RC circuit at the EN pin to slow down the voltage driving the enable pin because a…
Hi Dice-K,
TPS7A16A is a spin from TPS7A16A and there are some differences for the EN Voltage requirements and UVLO
TPS7A16A EN pin:
Compared to TPS7A16:
Also, notice the recommended slew rate for TPS7A16A. This question has been addressed several…