Part Number: TPS7A19 Hi team,
I have a question. Although the TPS7A1901 does not include an automatic discharge function, is it possible to implement a discharge function using the PG pin?”
Part Number: TPS7A19 Tool/software: The datasheet states in the description that the TPS7A19 maintains regulation during voltage transients by acting as a simple surge protection circuit. Are there any specifications for this feature? How high of a transient…
Part Number: TPS7A19 Tool/software: The datasheet recommends the value of (R1+R2) should be 10k-100k to avoid divider error, but there is no specification on minimum current required for the FB input. What is the minimum FB pin input current required…
Part Number: TPS7A19 Tool/software: Hi team,
Customer is evaluating TPS7A1901 to output 3.3V. If Vin is stable TPS7A1901 works correctly but the Vout become 5V when Vin is unstable. Why does TPS7A19 reach to 5V when the Vin is applied? It doesn't seem…
Part Number: TPS7A19 Tool/software: Dear TI Team,
Have you ever done some noise tests for PG pin floating scenarios? Our application limited the numbers of components. So we are expecting to leave PG pin floating without pull-up resistor, reducing…
Part Number: TPS7A19 Tool/software: Dear TI team,
For my application, maximum Vin=28V (nominal Vin=24V), Vo=3.3V, and Io is not more than 50mA.
And my application strictly limits the height of components, so I plan to use 0603 capacitors.
…
Part Number: TPS7A19 Tool/software: In the d/s, it says that output voltage regulation is +/-2% over temp. Is it including line regulation and load regulation? Thanks!
regards
Brian
Part Number: TPS7A19 Other Parts Discussed in Thread: TPS7A49 , TPS7B91 Tool/software: Hi LDO team,
I have an opportunity for a Wide vin LDO, the requirements are:
Vin = range between 10-36V
Vout = 5V
Iout - 50-100mA
As cheap as possible…
Part Number: TPS7A19
Hi support team,
In the "SUPPLY VOLTAGE AND CURRENT" item of SBVS256A, there is a description that the minimum input voltage value is "Vout + 0.5V". This value is the value when Iout = 450mA, and when using it at Iout = 100mA…