Part Number: TPS7A20 Hello,
My customer requested a review by TI regarding the TPS7A2018PYCKR.
Could you please review the design below to see if there are any issues?
Thank you.
Part Number: TPS7A20 I have a problem with the orientation of TPS7A2033PYCJR. I am in doubt if the A1 marker is the dot or the arrow. The dot is at A1 in the production. But It only works if it is turned 90 deg CCW
Part Number: TPS7A20 Tool/software: Hi team
we would like to know power dissipation, if Vin 3.3 and vout is 2.8V, Iout = 65mA
as per datasheet formula, we got 0.0325,
But component failing at 65 degree.
Please provide the siggestions
Part Number: TPS7A20 Hello,
I would like to know the meaning of the ".A" suffix in the MPN TPS7A2050PYCKR.A . Does it indicate a custom reel size?
If I would like to order a reel with 2,000 pieces , would the correct MPN be TPS7A2050PYCKR.2000 ? …
Part Number: TPS7A20 Regarding TPS7A20 Data Sheet(SBVS338D – MARCH 2020 – REVISED JULY 2021) At the beginning of Electrical Characteristics, It is written: "Vin = Vout(nom) + 0.3V or 1.6V, whichever is greater," If we use TPS7A20285, Vin=2.85V+0.3V=3…
Part Number: TPS7A20 Hi team,
Per our discussion, Could you please provide the FFT data for TPS7A20 within below parameter?
Input voltage:3.6V
Output voltage:2.8V
Output current:200mA
FFT and other scope setting:
Thank you,
Yishan C…
Part Number: TPS7A20 Hi ti team,
We are asking some question related for TI LDO TPS7A2011PYCKR.
Regarding the LDO (TPS7A2011PYCKR) top marking inspection issue (in our factory), can you share some information to us ?
What type of light source…
Part Number: TPS7A20 Hi,
I have a query from one of our customers in relation to the TPS7A2030PDQNR which we are considering to use in an application that we are putting together.
The question is in relation to Quiescent current/leakage when VEN …