Hi Dice-K,
While the current exceeds 520mA, it does so for a short enough time that the device will not increase in temperature enough to cause damage.
Best Regards,
Alex Davis
Part Number: TPS7A20 Tool/software: Hi Team,
Could you please tell me the output voltage tolerance under the condition of Vout < 1.8V, Vin = (Vout + 0.3V ) to 6.0V?
The other three conditions in the electrical characteristics table all have Vin = …
First, I will explain what I understand about the TPS7A20. Please point out any errors in this explanation.
The TPS7A20 turns off the MOSFET output when the input voltage is below VUVLO (1.17~1.59).
The TPS7A20's active discharge is enabled when VEN…
Part Number: TPS7A20 Tool/software: Hi Team,
Do you know at which output voltage the TPS7A20225PDQNR works?
At 2.25V or 2.5V?
Thank you.
Kind regards,
Wouter Kragt
Part Number: TPS7A20 Tool/software: Hi team,
Could you help share the difference between TPS7A2018PDQNRM3 vs TPS7A2018PDQNR?
Thanks and best regards,
Will
Part Number: TPS7A20 Tool/software: Hi,
Do we have X2SON package P2P device with TPS7A20?
Customer need high PSRR in low frequency, better same with 7A20. The output current can be lower.
Thank you,
Yishan Chen
Part Number: TPS7A20
Tool/software:
hello. In this project, the circuit was constructed using TPS7A20.
The current consumption of the load connected to the TPS7A20 does not exceed 10mA.
I am trying to turn the TPS7A20 output ON/OFF by controlling the…
Part Number: TPS7A20 Tool/software: Hi,
May I know there have alternative LDO for below Anasemi VRH series?
Iout = 250mA Vout = 3.3V, low dropout, PSRR~70DB, under 25uA
We found the closest is TPS7A20 series but
VRH3001NTX.pdf
Part Number: TPS7A20 Tool/software: Hello teams
Could you tell me the principles of an LDO?
An LDO has a built-in FET. The output of the error amplifier via a feedback circuit is connected to the gate terminal of the FET.
As you know, the FET controls…