Part Number: TPS7A24 Hi,
I am using LDO regulator in my design. I measured input voltage 5V and input current 20mA also measured output voltage 3.3V and output current 19mA. I think, It shouldn't be same current input and output.
I looked quiescent…
Part Number: TPS7A24 Hello
TPS7A24 datasheet defines C_OUT value as 1 ~ 100uF with note "(1) All capacitor values are assumed to derate to 50% of the nominal capacitor value".
Does that mean C_IN must be 1uF+-50% ~ 100+- 50% = 0.5uF ~ 150uF…
Part Number: TPS7A24 Dear Sir/Ms.
I have to download the TPA7A24XX PSPICE from the Ti website, but the default value is TPS7A2401. We did it a bit. There is no TPS7A2450. How can I change it to TPS7A2450? Or do you have a TPS7A2450 model?
Thank you
Kami…
Part Number: TPS7A24 Hi sir,
Regarding Cin value(Input capacitor) is typ. 1uF.
the note is that all capacitor values are assumed to derate to 50% of the nominal capacitor value.
what is Min value for Cin?
Thank you for your suggestion.
Regards,
Part Number: TPS7A24 Recommended values for output capacitors The data sheet has a range of MIN: 1uF, NOM: 2.2uF, MAX: 100uF. Under what conditions is this determined? (For example, it depends on the output current)
Also, what is the optimum value when the…
Part Number: TPS7A24 What is the range of output adjustment resistance of TPS7A2401DBVR?
For example, to output around 5.35V
Is it possible to set R1 = 56kΩ and R2 = 16.9kΩ?
(R1 and R2 follow the reference of the circuit described in the data sheet)…
Part Number: TPS7A24 Please confirm the error in the data sheet of TPS7A2401DBVR.
The calculation example in "8.2.2.2 Selecting Feedback Divider Resistors" is I think it is a calculation example of VOUT = 3.3V, so do you meet with the recognition…
Part Number: TPS7A24 Hello team,
What is the PCB layout for measurement of Rθja?
I read "Semiconductor and IC Package Thermal Metrics", but I could not find it.
My customer wants to know "number of layers" to consider their layout before…
Part Number: TPS7A24 Other Parts Discussed in Thread: TPS7A02 Is Iq of the TPS7A24 not modeled? I put together the following simulation to create a precision 1 uA current sink and the Iq of the TPS7A24 is more than 10 times the expected value. Seems like…