Part Number: TPS7A25 I have a quick question regarding the internal feedback resistors on the fixed output versions of the TPS7A25.
For a 5V output what are the resistor values, power ratings, and tolerances.
Best Regards,
Nick Haneline
Part Number: TPS7A25 Hi Sir/Madam,
i check the TPS7A25 datasheet.
i have a source 12Vdc. output around 3.3 V / 1A.
1.
T A(MAX) = T J(MAX) – (R θJA × P D )
T A(MAX) =125°C – [73.3°C/W × (12 V – 3.3 V) × 0.09 A] = 70.2°C…
Part Number: TPS7A25 Hello Team,
the pSPICE simulation only works for Vout=1.24V. As soon as I add a voltage divider to the FB pin nothing works(= no output voltage).
Thanks for your help!
Hans
Part Number: TPS7A25 I'm using TPS7A2533.
I have the following questions about soft start and inrush current.
●The datasheet says that the soft start function is built in, but where exactly is it built in the block diagram?
●Is the soft start function…
Part Number: TPS7A25 Hi,
I am planning on using TPS7A25 in an application which imposes a limit on total capacitance allowed during initial turn-on for the first 20ms to avoid tripping of the upstream inrush current limiter. How can I compute the total…
Part Number: TPS7A25 Hi team,
Customer is wondering why several Mohm resistor is used for feedback instead of kohm resistor.
Could you kindly share the reason why ?
Thank you and best regards,
Michiaki
Part Number: TPS7A25 Hello expert,
My customer is using TPS7A2501 in their IPC application. Please see below waveform OCP and soft start period. It seems like voltage is over customer's spec during these two conditions. May I know if you can help to double…