Part Number: TPS7A30-49EVM-567 Other Parts Discussed in Thread: TPS7A49
We tested the load regulation for TPS7A30-49EVM-567 on default setting, these spec was out of range the datasheet specification below.
Please let me know about three points be…
Part Number: TPS7A30-49EVM-567 Other Parts Discussed in Thread: TPS54060EVM-590 Hi TI team,
We bought TPS54060EVM-590 and tested with LDO TPS7A30-49EVM-567. They are working great!
Now we will integrate them two into our design. Could you help to share…
Part Number: TPS7A30-49EVM-567 In the User's Guide (SLVU405–August 2010) for the board it is recommended, that +/-18V is used for the initial operation. In my application I have a fixed voltage source for Vin of +/-24V which is controlled manually, using…
Part Number: TPS7A30-49EVM-567 Other Parts Discussed in Thread: TPS7A30 A TPS7A3001 is wired for a -5V output. R1 and R2 are selected to achieve a -5V output. However, Vout equals -3.9V instead of -5V.
When SW1 is opened, the output changes to -12V…
Part Number: TPS7A30-49EVM-567 Other Parts Discussed in Thread: TPS7A49 , TPS7A30
The datasheet of the TPS7A30-49EVM-567 evaluation board has an equation containing a value called Fz. The value Fz is not provided in the TPS7A3001 datasheet or the evaluation…
Hi Adam,
I would use this EVM here it is for the TPS7A30, which has a very similar pinout. Typically for negative LDOs we recommend the use of TPS7A30 as you get the NR/SS pin included.
https://www.ti.com/tool/TPS7A30-49EVM-567
I am working on getting…
Part Number: TPS54060EVM-590 Other Parts Discussed in Thread: TPS7A30-49EVM-567 , , TPS54060EVM-457 Hi TI team,
We bought TPS54060EVM-590 and tested with LDO TPS7A30-49EVM-567. They are working great!
Now we will integrate them two into our design. Could…
Hi Yu,
I was actually able to get to this today.
I reproduced the spikes you are seeing using the TPS7A30-49EVM-567. I used the default capacitors on the board.
I tried removing all of the capacitors on the board, hoping that I could filter out the…
Hello,
A good low noise lab supply with multiple outputs should work well. However, you can also use individual LDO's, which is how you would power the device when designing your own board.
TPS7a3001 and TPS7a4901 are good options for the +9V and…
Part Number: TPS7A49 Other Parts Discussed in Thread: TPS7A30-49EVM-567 , The datasheet of the LDO TPS7a49 specifies a limit of -36 ... 0.3V for the OUT pin to IN pin voltage. I am using the regulator with a relatively large output capacitance of 1mF and…