Part Number: TPS7A3001-EP Hi Team,
I'm planning to use TPS7A3001 in my board.
The below mentioned is the power and noise requirement in my board.
Noise or ripple on any power rail or reference voltage shall not introduce discrete spectral components…
Part Number: TPS7A3001-EP Tool/software: Using TI spice, the part ramps up to a 3V output no faster than about 1msec, with no SS/NR cap installed.
But according to the data sheet formula below:
if iCL max = 330mA (typ.) Vo should ramp up in…
Part Number: TPS7A3001-EP Tool/software: The TPS7A3001-EP data sheet indicates the reference voltage is Minimum -1.22V, Nominal -1.184V and maximum -1.142V. The graph in figure 2. shows VFB being near -1.175V at 25C. There appears to be an offset between…
Part Number: TPS7A3001-EP Tool/software: Dear Texas,
I am looking for the following information, end of life, mean time between failure, mean time to failure on the following components:
TPS7A3001DGNT
TPS7A4901DGNR
LM3940IMP-3.3/NOPB
TLV117125DCYT…
Part Number: TPS7A3001-EP Other Parts Discussed in Thread: TPS7A30 , TPS7A49 Hi Team,
Can you please help with the inquiry below?
In the datasheet, the enable pin has a maximum rating of +36V to VIN or +36 / -36 V to GND. In the electrical characteristics…
Part Number: TPS7A3001-EP I have TPS7A4901DGNT and TPS7A3001MDGNTEP LDOs. Voltage drops are 5 V and 2 V respectively. Should I use heatsink with this parts?
Sincerely,
Behtan Umut Mercan
Part Number: TPS7A3001-EP Other Parts Discussed in Thread: TPS7A30 Hi,
I am trying to substitute the linear voltage regulator, TPS7A3001DGNR, and came across a part in the same family, TPS7A3001MDGNTEP. I examined both datasheets and I can't seem…
Part Number: TPS7A3001-EP Hi,
The packaging drawing (HVSSOP (DGN)) for this part does not have a minimum drawing callout - is that information available? We are interested in order to select the correct thermal gap pad thickness.
Thank you!
…