Part Number: TPS7A3501 Other Parts Discussed in Thread: TLV767 Tool/software: Is the TPS7A3501 reliable for long-term operation at 5.5V at room temperature ,? given that its recommended operating voltage range is 1.71V to 5V and its absolute maximum rating…
Part Number: TPS7A3501 Good day, I am trying to replicate Figure 13 to verify the performance of a noise measurement circuit. I am using an RSA5103 spectrum analyzer and am able to obtain the same shape as in Figure 13. However, after performing conversions…
Part Number: TPS7A3501 Hello,
It's clear that reverse current should be avoided. However, is there some safe limit of reverse current, which can flow through the device during shutdown, without causing damage to the LDO?
Thank you in advance!
J…
Part Number: TPS7A3501 Hello All, for the part TPS7A3501, the datasheet specifies a block diagram, can anyone help to understand how is this working. Is the opamp indicated in the block diagram a simple opamp or is there any level shifter kind of structure…
Hi Kevin,
The TPS7A3501 does not have a boost function. When you set the delta V to 500mV that causes the power filter to regulate the drop from Vin to Vout to be 500mV. So if you want Vout=1.8V then you will need to set Vin=2.3V.
Part Number: TPS7A3501 Dear e2e Support,
Could you tell us if there is a typo mistake in our datasheet, page 9 & 10, graph 18 and 19 specifically, about the 2V/div legend?
Graph 18 for example, 2V/div would mean that Vin goes from 0 to 5V, while…
Part Number: TPS7A3501 I am planning to use TPS7A3501 (Power filter). I was wondering: If the load current is much less than the 1A limit, (lets say 200mA) would it be possible to program the dropout to less than 200mV? From the circuit diagram, this…
Part Number: TPS7A3501 Hi,
We are designing a power supply for HiFI audio, so we need the rms noise performance in 20 to 20KHz, could you please help to provide it? I only see the noise from 10Hz to 100kHz is 3.8uVrms. Thank you.
Other Parts Discussed in Thread: TPS7A3501 Hello
I have a question.
device:TPS7A3501 Please see datasheet P11.
8.2.2.5 Start-up time Equation (3) T_startup = 250,000 × CNR (s)
The calculation value is wrong with the actual, but why is it?
Details…