Part Number: TPS7A39 Other Parts Discussed in Thread: TPS7A33 hi sir
that the TPS7A39 is a good device, but the current output is small
could I use the Twice Tpas7a39 to double the output current?
need +300mA
thanks
Part Number: TPS7A39 Dear Team,
Do we have suitable solution can replace TPS7A3901DSCR? because lead time of this one is too long...(We need supply better than this one)
Many Thanks,
Jimmy
Part Number: TPS7A39 I have some questions/problems regarding to TPS7A39 regulator. According to the datasheet, VNR/SS Internal reference voltage is between1.17V and 1.208V.
But I measured on my board, it is 4.4V (IC batch 1) and 1V (IC batch 2). I am…
Part Number: TPS7A39 Hi team
We need the Dual supply LDO which converts the 3V to + 2.5V and -2.5V with smallest Package. We have found the TPS7A39 but it is out of stock now. Could you please suggest me the part which can give the dual output
Part Number: TPS7A39 Hi,
As title, I would like to know TPS7A39 suitable for this application?
1. Vin 21.7~22.3V to Vout 14.5~15.5V
2. Vin -7.3~-6.7V to Vout -13.5~-12.5V
Thanks!
Jeff
Part Number: TPS7A39 I'm having a bit of trouble with an LDO specifically TPS7A39. I'm having very inconsistent success in its implementation I have have several failures where the positive side output is the positive supply voltage and the negative output…
Part Number: TPS7A39
Hi,
Currently, the VIN pin of the TPS7A3901DSCT fails due to overvoltage in products after mass production.
I would like to share detailed circuit diagrams and layouts and ask questions, so is it okay if I send you a private message…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: INA821 , TPS7A39 , INA823 I use TPS7A39 to supply +-5V power supply to INA821, when I run Time Domain simulation, he says there is convergence, and it takes 20 seconds to calculate the solution…