Part Number: TPS7A4001 Hi Team
The gap between the chip pin pads is only 0.2mm, and the input voltage is 100V. Is there any creepage distance problem?
Best Regards
Gene
Part Number: TPS7A4001 Hello Experts, My customer is considering to use TPS7A4001. He would like to confirm whether the attached circuit will work correctly or not. Would you please review it? Question_TPS7A4001_(09142020).xlsx Best Regards, Fujiwara
Part Number: TPS7A4001 Hello
Since working with this regulator for telecom's radio head equipment development, I notice how sensitive the IC feedback path is to a local RF field over the cell-phone frequencies.
To minimize the sensitivity, feedback…
Part Number: TPS7A4001 Hello team,
Can the TPS7A4001 be used as a constant current source similar to other LDOs? and if so is this the correct way of doing it?
Thanks in advance.
Part Number: TPS7A4001 In our Application,
Input Voltage = 65V
Output Voltage = 5V
Input Cap= 1uF
Output Cap= 10uF
R1= 100 K (//10nf)
R2= 30K.
We observe, some noise get coupled at output 5V & Feedback Pin, which causes drop in output voltage…
Part Number: TPS7A4001 Hi,
I have a requirement where I would like to use the TPS7A4001DGNR to generate the variable voltage from 85V to 90V based on my input voltage which can vary from 88V to 92V.
Is it possible to do the above variations with…
Part Number: TPS7A4001 Dear Sir,
Could you please suggest any similar part with Max Input Voltage 100V and Output 12V / current minimum 75mA or more.
Operating Temperature is –40°C to 125°C .
Thanks and Regards,
Nesh
Part Number: TPS7A4001 Other Parts Discussed in Thread: LM2936 , In our Application,
Input Voltage = 65V
Output Voltage = 5V
Input Cap= 1uF
Output Cap= 10uF
R1= 100 K (//10nf)
R2= 30K.
we used this device in our Transmitter Product, The…
Hi Koho,
To verify this function, it's better to use a DC source to replace the DAC during debugging. You may then run DC transfer characteristic sims by varying the VG1. Please see the results also in the screenshot. As you can see, when VG1 is varying…
Part Number: TPS7A4001 Hi, I need a simple LDO to deliver a 3.3V supply for the control circuits of a medium voltage load switch. The current levels under normal operation from this 3.3V supply will be just a few 100 uA. I was therefore hoping to get…