Part Number: TPS7A4101 Hi Team,
Good day!!
Kindly proivde the COD(Country of Diffusion) for the below MPNs:
TPS7A4101DGNR
TLV333IDCKR
TPS79850QDGNRQ1
THVD1550DR
THVD1550DR
UCC28C45QDRQ1
TPS70933DRVR
…
Part Number: TPS7A4101 I am planning on using the TPS7A4101 as an 48V LDO from a 48.3V input with a load of 20 mA. It looks like this part will do that. Is there a reason why this part is not listed as a featured LDO? Is there a new part that will replace…
Part Number: TPS7A4101
Tool/software:
Dear Technical Support, Good day! Please verify for TPS7A4101DGNR the reported EXPOSED THERMAL PAD oxidation if any concern to further use.
All our remining stock is verified to have the same condition.
Per…
Part Number: TPS7A4101 Tool/software: Hello Team,
Greetings for the day!
We are planning to use LDO "TPS7A4101DGNR" for 10V regulation from Input supply range of 13V to 35V. We are not clear on the following statement for the total feedback resistance…
Part Number: TPS7A4101 Other Parts Discussed in Thread: TPS7A44 , TPS7A30 , LM1085 Dear Team,
Do we have any LDO solution can meet the spec as below?
Vin=48
Vout/Iout= 28V(2A), 5V(30mA), -7.5(10mA), -3.4(10mA)
Many Thanks,
Jimmy
Part Number: TPS7A4101 Other Parts Discussed in Thread: TINA-TI Hi Team,
In my V-I circuit design based on amplifier, i need convert the 24V power to 3.3V and run the simulation in TINA, but unfortunately i can't find the
TPS7A4101 tina simulation…
Part Number: TPS7A4101
I did a simulation in WEBENCH POWER DESIGNER as you can see below.
In this simulation the results for input and output current were not correct, since 10mA input current results in 50mA output current. This should be impossible…
Part Number: TPS7A4101 Hi team,
My customer found that the load transient response of TPS7A4101 is very slow.
After a while from the start-up, when the load step from 0 A to several tens of mA occurs, it took several ms to settle to the target output…
Part Number: TPS7A4101 Dear experts,
Could I ask what will happend on the Vout if the Vin equal to 5V for the TPS7A4101 with feedback resistor 480K (To Vout) and 20Kohm (to GND)?
Thanks!
Dylan
Part Number: TPS7A4101 Other Parts Discussed in Thread: LM358B Dear teams,
I am planning to use TPS7A4101 with Vin (max=48V), Vout (30V), Iout (0.4mA max). This LDO output will go to the V+ (Supply voltage) of op-ap LM358B. Could you help check whether…