Part Number: TPS7A4101 Other Parts Discussed in Thread: TPS7A44 , TPS7A30 , LM1085 Dear Team,
Do we have any LDO solution can meet the spec as below?
Vin=48
Vout/Iout= 28V(2A), 5V(30mA), -7.5(10mA), -3.4(10mA)
Many Thanks,
Jimmy
Part Number: TPS7A4101 Other Parts Discussed in Thread: TINA-TI Hi Team,
In my V-I circuit design based on amplifier, i need convert the 24V power to 3.3V and run the simulation in TINA, but unfortunately i can't find the
TPS7A4101 tina simulation…
Part Number: TPS7A4101
I did a simulation in WEBENCH POWER DESIGNER as you can see below.
In this simulation the results for input and output current were not correct, since 10mA input current results in 50mA output current. This should be impossible…
Part Number: TPS7A4101 Hi team,
My customer found that the load transient response of TPS7A4101 is very slow.
After a while from the start-up, when the load step from 0 A to several tens of mA occurs, it took several ms to settle to the target output…
Part Number: TPS7A4101 Dear experts,
Could I ask what will happend on the Vout if the Vin equal to 5V for the TPS7A4101 with feedback resistor 480K (To Vout) and 20Kohm (to GND)?
Thanks!
Dylan
Part Number: TPS7A4101 Other Parts Discussed in Thread: LM358B Dear teams,
I am planning to use TPS7A4101 with Vin (max=48V), Vout (30V), Iout (0.4mA max). This LDO output will go to the V+ (Supply voltage) of op-ap LM358B. Could you help check whether…
Part Number: TPS7A4101
Hi sir,
This is Bhuvaneswari from Zettaone Technology,
I need to know few details for the part TPS7A4101DGNT
Parts are currently active in the website, may i know how long it will be in production? Is there any EOL issued for this…
Part Number: TPS7A4101 To USA FAE whom will be concern: HI, the back of chip with obvious water mark for the P/N TPS7A4101DGNR, and we want to know if it is normal condition ? we are looking forward to your feedback ASAP. Thanks!
Part Number: TPS7A4101 Other Parts Discussed in Thread: LM5001 Hi,
I am looking to simulate TPS7A4101 and LM5001 using ltspice. I was looking for the unencrypted model that can be imported into Ltspice.
I am able to use these models in PSpice for TI…
Part Number: TPS7A4101 Hi team,
Can the TPS7A4101 6pin and 7pin be shorted to the VIN?
The reason for asking this question is that my customer used the TPS79801 in old projects and shorted 6pin and 7pin to…