Part Number: TPS7A47 Hi Team,
I find the most parameters of TL1963ADCQR and TPS7A4501DCQR are the same although they are different series of TL and TPS. What's the difference between them? Why do so similar two chips belong to different series?
Beat…
Part Number: TPS7A45 Hi Team,
We are using LDO TPS7A4501DCQT in one of our project our requirements is VIN - 13V Vout - 11.5 Iout - 1.5A our ambient temperature is 25°C to 50°C. In datasheet mentioned Junction-to-ambient thermal resistance - 50.5°C…
Part Number: TPS7A45
Hi, my design with TPS7A45 is as following.
But when Pin1 is LOW to disable TPS7A45, the output is around -0.5V. I also tried to put 500 Ohm at pin4 to provide load, but doesn't make any improvement.
How to prevent negative…
Part Number: TPS7A45 DO we have a 3.3V -> 1.8V / 500mA LDO with enable where the PG Output is independent of the EN pin?
For instance, if the LDO is turned off via the EN pin, will the PG stay active until the output discharges below, say 95% of the…
Part Number: TPS7A45 I'm measuring 1.6V at pin#5, ADJ, as opposed to 1.2V. the same circuit works ok on the other board. is there any way to troubleshoot the problem? what could have caused the issue? it's not easy to just take the part off the board…
Part Number: TPS7A45 Hi, Could you tell me about TPS7A45 reverse current operation? Customers are considering the following diode installations. The background is to prevent the output voltage from rising during reverse current protection. Should customers…
Hi Aaron,
Ok, I'll try and identify some specific part numbers and get back with you. I also have a couple of more similar questions about some other parts. I'll send these questions to your e-mail address.
I appreciate your help.
Regards…
Part Number: TPS7A45 Hello there,
I found a previous thread somewhat helpful as it clarified that the TPS7A45XX has current limiting protection which limits the output current depending on Input-Output differential voltage and ambient free air temperature…
Part Number: TPS7A45 I have a TPS7A4533 voltaje regulator, my question is: can I use it in Dropout Operation mode?, i.e. can I input 3.3V and obtain 3.3V at ouput?
Part Number: TPS7A45 Asking this for my customer...
I am looking into improving the phase noise by adding feedforward capacitance. The data sheet on this part seems to lack context—on page 19, it goes through a calculation or two regarding poles and…