Part Number: TPS7A47 Other Parts Discussed in Thread: TPS7A33 Hi,
I have configured a TPS7A4700 to provide an output of 12 volts. The input voltage is +15V, from a linear benchtop supply.
When load current is less than 100mA, the output voltage is…
Part Number: TPS7A47 My customers are using the TPS7A4701, and over the past half years, they have been getting 4 to 5 pcs failure IC from their end customer side, and replace a new chip can solve the issue. So they would like to request our support on…
Part Number: TPS7A47 I am planning on using this RF LDO (TPS7A4700) to convert 28V into a precision 10V power rail for a sensor. The device functionality depends on some pins being left floating when using the ANY_OUT feature to set the output voltage…
Part Number: TPS7A47 Tool/software: Hello:
The schematic diagram of LDO is as follows: TPS7A4701RGWR
The PCB part is as follows:
The following is the debugging process:
Board level testing shows output ripple:
There is a ripple of 10…
Part Number: TPS7A47 Tool/software: Hi,
We are using TPS7A47 for generating +5V.Input voltage is +5V.
Output current requirement is 1 A .
Kindly review the attached schematic and provide the feedbacks.
Regards,
Ashish
8816.Review-2.pd…
Part Number: TPS7A47 Other Parts Discussed in Thread: ADS1220 , LP2951 , Tool/software: Hello, I am looking for a supply with a Vout of 3.3 V for the AVDD of the ADS1220 ADC. Currently, I have Vin = 24 V, from which I derive the 3.3 V for the entire PCB…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Tool/software: Hi team,
I want to perform BODE analysis on the following circuit using TINA.
This circuit uses TPS7A47-Q1 as an LDO regulator and connects it in parallel with an NMOS…
Part Number: TPS7A47 Tool/software: Hello,
I am an FAE at a distributor that handles TI products. I have received some questions from my customer about the TPS7A4701. (Question 1) It generates +5V from +12VIN. If a voltage of -0.4V to 36V is applied…