Part Number: TPS7A47-Q1 Hi team,
When I add the input from 5V to 20V and the output is kept at 3.3V, is it normal for the device temperature to go from 30 degrees to nearly 100 degrees?
If the maximum input voltage of the device of 35V needs to be…
Part Number: TPS7A47 Hi team,
My customer is using LT3042 now.
And I wonder if we have a device to replace it, I saw TPS7A47(5mm*5mm), but it is bigger than LT3042 (3mm*3mm)
Requirements:
High PSRR
Enable pin
small size
Thanks,
…
Part Number: PMP8372 Other Parts Discussed in Thread: TPS7A47 , TPS7A33 , PMP
Team,
Question about the TPS7A47 / TPS7A33 LDOs used in https://www.ti.com/tool/PMP8372 :
-Is it possible to use two TPS7A47 and two TPS7A33 in parallel to lower the current…
Part Number: TPS7A47 Hi
My question is regarding the TPS7A4700, datasheet rev SBVS204F. I am getting most of the DC parameters to pass in my testing with the exception of the following fails ---> overall_accuracy and current limit at Vin/Ven = 3V. If…
Part Number: TPS7A47
Hello team, My customer has a question about noise performance vs Output Capacitor value. Would you please share the noise performance in case of Cout = 10uF case?
In ds, the following is described. 8.2.2.1.1 Input and Output…
Part Number: TPS7A47 We're considering using an ANY-OUT LDO and an I2C IO Expander, such as outlined in appnote SBVA035A, to change the LDO output setting under firmware control. What's not clear to us is if this can be done on the fly, while the LDO…
Part Number: TPS7A47
Hi team,
my customer is looking for a LDO supply MOS for relay in the EV charging.
TPS7A47 is thermal is low, is it be qualified?
or do we have better solution?
Vin:12V
Vout:6V
Iout:0.3A
Part Number: TPS7A47 Other Parts Discussed in Thread: TPS7A33 , PMP Team,
Question about the TPS7A47/TPS7A33 LDOs used in https://www.ti.com/tool/ PMP8372 :
-Is it possible to use two TPS7A47 or two TPS7A33 in parallel to lower the current/power dissipation…
Part Number: TPS7A47 Hi,
I have a reel of TI P/N TPS7A4700RGWR that seems to have 2 different Date markings within the reel. Is this normal?
And we have the following markings
As far as I know, work days for week 26 run from Monday June 27th…
Part Number: TPS7A47 Other Parts Discussed in Thread: , TPS7A85 Hello all -
I require a high current and low noise (High PSRR + low output noise) 7.5V supply that is capable up to about 2A. We also require good transient response ~100mV pk-pk change…