Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Hi,
When TPS7A47's output is short when VIN=36V, VOUT=1.4V and IOUT is short. Therefore the power dissipation on pass FET will be about 36*1.26=45W. Will thermal shutdown protects the device…
Part Number: TPS7A47-Q1
Hi Team,
My customer is using TPS7A47-Q1 and recently reports 5 failure cases (in total 30 boards).
Background:
1) Input voltage: 24.5~28V (Input comes from the multi-windings Flyback, it's the aux-winding output and varies due…
Part Number: TPS7A47-Q1 Hi Team,
My customer use TPS7A47-Q1 in his automotive project.
He use it in a 10Vin / 9Vout 500mA Max. load design.
Now he had a output keep short to GND test, need to make sure our device safety include the thermal perform.
He…
Part Number: TPS7A47-Q1 Hi team,
My customer would design TPS7A4701QRGWTQ1 in his project.
Do we have the TPS7A4701QRGWTQ1 Maximum & Minimum value of VREF can provide to customer?
Thanks!
Kai
Part Number: TPS7A47-Q1
I am using the voltage regulator for 3.3V output. Below is the circuit I am using.Issue I am facing is that whenever I give Vin =25V from battery source.The regulator gets burnt.Due to this my MCU gets damaged aslo.Please suggest…
Part Number: TLV766-Q1 Other Parts Discussed in Thread: TPS709 , TPS7A20 , TPS7A47 , TPS7A24 Hi team,
TLV766-Q1 requires 2mΩ ESR as recommended operating condition.
While, the datasheet also states that "The device is designed to be stable using low…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Hi team,
May I have your help to propose the LDO solution automotive solution to meet below requirements?
Vin = 10.5V
Vout = 10V
Iout = 1A
AEC-Q100 is needed
Is TPS7A47-Q1 the best solution…
Part Number: TPS7A47-Q1 When using the adjustable feature on the TPS7A47-Q1, is the output accuracy determined solely by the accuracy of the set point resistors or do I need to consider overall accuracy, line regulation, load regulation specs?
Also,…
Part Number: TPS7A47-Q1 Hi Power Management team, I am attempting to use TPS7A47-Q1 to regulate 30V (Pins 13, 15, and 16) down to 25V using its Adjustable Operation. Can you please review the schematic below and respond with comments of recommended changes…