Part Number: TPS7A47-Q1 When using the adjustable feature on the TPS7A47-Q1, is the output accuracy determined solely by the accuracy of the set point resistors or do I need to consider overall accuracy, line regulation, load regulation specs?
Also,…
Part Number: TPS7A47-Q1 Hi Power Management team, I am attempting to use TPS7A47-Q1 to regulate 30V (Pins 13, 15, and 16) down to 25V using its Adjustable Operation. Can you please review the schematic below and respond with comments of recommended changes…
Part Number: TPS7A47-Q1 Hi All,
I am planning to use this part as a programmable LDO between 1.7-5.5V. (The current that I might draw is approximately 50mA in these operating voltage range) The problem is that the environment in which i am using the has…
Part Number: TPS7A47-Q1 Hello,
Mu customer uses TPS7A4701-Q1 from Vin=6V to Vout=4.5V and checked the output timing. Would you please give me your comments?
1. They checked the output and found it took around 3ms from EN=1 to start Vout rising. They'd…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TIDA-01232 We have tested the TPS7A47-Q1 LDO voltage regulator and it has excellent performance for our application of filtering the output of our DC-DC Converters (< 1mV rms output ripple measured…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 , TPS7A33 , LM337-N Hello!
I need a negative voltage regulator with input voltage -35V output current 1A with the same noise parameters such as the TPS7A47 Voltage Noise: 4.2 μV RMS (10 Hz…
We don't have anything more modern in that metal can, but here is a link to a filtered version of our parametric search which shows the positive voltage linear regulators that we do have in a metal can.
If you wanted to assess newer options I'd start…
Part Number: TPS7A47-Q1 Hi
We have the application with limited space on RF/Microwave hybrid frequency upconverter (hybrid means chip/die connecting by gold bond wire)
The maximum space allowed is 0.2 inch square while this QPN package dimension is 0…
Part Number: LM1084 Other Parts Discussed in Thread: INA253-Q1 , , INA745B , TPS7A47 , TPS7A85A , TPS7A84A , TPS7A57 , TPS7A54 , TPS7A52 , TPS7A53 Tool/software: I am reaching out regarding a design challenge in my application and would appreciate your assistance…