Part Number: TPS7A4701-EP I download the transient model for the tps7a4701 and used the .tsm file to create the model on TINA-9. When the I set the circuit up for astable operation, the transient analysis creates a plot where the y axis is all a single…
Part Number: TPS7A4701-EP Other Parts Discussed in Thread: TPS7A47 Hello,
Can you tell us when bringing EN (low) how long before the output is off? We would like to understand typical and range and what is actually determining the time. Today we observe…
Part Number: TPS7A4701-EP Hi All,
I want to use the TPS7A4701 LDO in adjustable through resistor mode. What should i do with the programmable pins for best design? (Do u suggest me to leave it floating?)
Part Number: TPS7A4701-EP Hi ,
One of my customer met the problems when using the TPS7A4701, and the problem shows as follow:
Vin 12V, Ven=2.4V,they want use the feedback resistors to get the Vout =7V, and the R14=50K, but there is no output signal!! Here…
Part Number: TPS7A4701-EP Hello,
I am currently working with the tps7a4701. Here is the schematic.
The 28V bus is attached to a battery, which can vary from 26V to 32V. The issue we are seeing is that every once in a while the part will die. We will…
Part Number: TPS7A4701-EP Hi
I am using the part with the adjustable output. I have 25V in and need 24V out.. But when I power up the output isnt stable. Its moving around a lot. Sometimes I get the same output as the input. Other times its around 24V…
Part Number: TPS7A4701-EP Hi Team,
A customer I'm supporting has inquired regarding the behavior of the device when operating in current limit mode.
To my memory, we provided similar details for the TPS7A3301 as the over current limit values weren…
Hey Thomas,
Can I ask why you are using the TPS7A4701-EP then?
The -EP signifies an increased temperature range among other things including an increase in price.
Are you looking for commercial grade products?
Thanks,
Daniel
Part Number: TPS7A4701-EP Other Parts Discussed in Thread: TPS5410-EP , TPS57140-EP Hi everyone,
I would like to design a product which needs RF power circuitry.
Input is 24V. Firstly, I need to use DC-DC converter, then I'll add LDO to the output of…
Part Number: TPS7A4701-EP Other Parts Discussed in Thread: TPS7A47 The Electrical Characteristics table lists the current limit for the TPS7A4700 / 4701 as 1A minimum and 1.26A typical. This is noted to be when intended drop is 1V and Vout drops to 90…